PCAL6408a power sequence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCAL6408a power sequence

ソリューションへジャンプ
2,113件の閲覧回数
thomaskofoedhan
Contributor III

Are there any known requirements to power sequencing between the 2 power rails of PCAL6408?

Thomas

タグ(1)
0 件の賞賛
返信
1 解決策
1,996件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Thomas,

There is no power sequence requirement for these two power rails. If I/O interface is not powered then nothing works since core operation is from I/O power (VDDP) and POR circuitry is also off.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,997件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Thomas,

There is no power sequence requirement for these two power rails. If I/O interface is not powered then nothing works since core operation is from I/O power (VDDP) and POR circuitry is also off.

Best regards,

Tomas

0 件の賞賛
返信