PCAL6408a power sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCAL6408a power sequence

Jump to solution
2,116 Views
thomaskofoedhan
Contributor III

Are there any known requirements to power sequencing between the 2 power rails of PCAL6408?

Thomas

Tags (1)
0 Kudos
Reply
1 Solution
1,999 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Thomas,

There is no power sequence requirement for these two power rails. If I/O interface is not powered then nothing works since core operation is from I/O power (VDDP) and POR circuitry is also off.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
1 Reply
2,000 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Thomas,

There is no power sequence requirement for these two power rails. If I/O interface is not powered then nothing works since core operation is from I/O power (VDDP) and POR circuitry is also off.

Best regards,

Tomas

0 Kudos
Reply