PCA9615 Failures

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9615 Failures

12,585 Views
Staff
Contributor I

Hi, Forum,

The circuit below is used on both ends of a 10-foot cable.  The PCA9615 I.C.s catastrophically and permanently fail, sometimes at both ends of cable simultaneously.  Failed I.C.s drag down our power supply and get hot - they die. Replacing the I.C.s fixes the problem.

Failures may occur after hours or days of normal operation, or immediately after a disconnect/reconnect, and possible after (unauthorized) hot-swapping.  The cable carries the PCA9615 dual differential bus, ground, and +24V.  +5V and +3V are generated from +24V independently at each end of the cable.  We are not using the hot-swap logic, but have EN tied to +3.3V.  The datasheet includes no Limiting Values identified for hot-swap, and its hot-swap description mentions nothing about protecting the I.C., so I presume the hot-swap logic is intended not to protect the device from damage, but to prevent the device from corrupting data when connected to a live bus.

The failure can be recreated by intentionally hot-swapping under ESD-safe conditions, so failures are probably not likely cause by ESD.

No microcontroller is available to operate the hot-swap EN signal at one end of the cable.

Is hot-swapping without using the hot-swap logic known to cause device failures? 

What is the failure mechanism?

The PCA9615 is a nice, inexpensive, compact solution to extending I2C through a cable.  We'd like to keep using it, and we want to keep using it if possible.

Suggestions?

Staff_3-1625341932550.png

 

 

 

Tags (1)
0 Kudos
Reply
4 Replies

11,729 Views
Satyabobbadi
Contributor I

I am also facing the same issue, can this be recovered with a power cycle? how to resolve the issue if the communication is throwing an error during the hot swapping. please clarify in detail.

0 Kudos
Reply

12,186 Views
jmse
Contributor I

I also have the same issue, VDDA = 3.3V, VDDB= 3.3V. and it all seems to be happening during hot plugging operations (also under ESD safe environment). Once the PCA9615 fails it won't recover, and the PCA9615 starts getting really hot.

0 Kudos
Reply

12,430 Views
aferm
Contributor II

I am having similar issues with heat and communication failure. VDD(A) = 3.3V, VDD(B) = 5V, EN = floating, no hot-swap.

0 Kudos
Reply

12,557 Views
guoweisun
NXP TechSupport
NXP TechSupport

For the unused of hot swap function, floating the EN pin because of it connect with VDDA inside of IC.

 

0 Kudos
Reply