Executing commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Executing commands

1,032件の閲覧回数
tonyZ
Contributor I

Hello all, 

 

I see that in the "NTAG 424 features and hints" document there are many references to commands. Are these commands the type that would be executed in a cli? If so how do you config environment to execute commands?

 

Thanks, 

 

Tony

タグ(1)
0 件の賞賛
返信
1 返信

1,003件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir this is Fabian,

Thank you very much for contacting us.

These aren't commands that are intended to be executed directly into a CLI.

These commands are intended to be sent by an NFC Reader to the NTAG 424. We highly recommend to use RFIDDiscover for configuration of the tag and, command exchange.

These commands are part of the ISO7816-4 and ISO14443 specifications.

Additional to this, we do provide an NFC Reader Library in case you are interested in building your own application with our NFC Readers.

Best Regards,
Fabian
0 件の賞賛
返信