PCA9614

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
3,749 Views
sd23
Contributor I

How do we determine termination resistor values for PCA9614?

0 Kudos
Reply
1 Solution
3,711 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sedef,

I would recommend you to take a look at the AN847 which includes the calculations of proper bus termination resistors.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
5 Replies
3,712 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sedef,

I would recommend you to take a look at the AN847 which includes the calculations of proper bus termination resistors.

Best regards,

Tomas

0 Kudos
Reply
1,752 Views
Mietto2
Contributor I

Hi,

I have a similar application with Vdd=3.3V on both sides, and Z0=100R.

Going through the app note, two questions arised:

1) The app note mentions the FAILSAFE bias = 200mV. What is that value with the PCA9614?

2) The app note do not consider 3 resistors on both sides of the cable, while the PCA9614 asks for that. What is the impact?

Best regards.

0 Kudos
Reply
3,700 Views
sd23
Contributor I

Thank you Thomas.

0 Kudos
Reply
3,746 Views
guoweisun
NXP TechSupport
NXP TechSupport

The termination resistor determined by the VCCA/VCCB setting,what're value of them in your side?

0 Kudos
Reply
3,732 Views
sd23
Contributor I

Both are 3.3V.

0 Kudos
Reply