PCA9614

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
3,800 次查看
sd23
Contributor I

How do we determine termination resistor values for PCA9614?

0 项奖励
回复
1 解答
3,762 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sedef,

I would recommend you to take a look at the AN847 which includes the calculations of proper bus termination resistors.

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,763 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sedef,

I would recommend you to take a look at the AN847 which includes the calculations of proper bus termination resistors.

Best regards,

Tomas

0 项奖励
回复
1,803 次查看
Mietto2
Contributor I

Hi,

I have a similar application with Vdd=3.3V on both sides, and Z0=100R.

Going through the app note, two questions arised:

1) The app note mentions the FAILSAFE bias = 200mV. What is that value with the PCA9614?

2) The app note do not consider 3 resistors on both sides of the cable, while the PCA9614 asks for that. What is the impact?

Best regards.

0 项奖励
回复
3,751 次查看
sd23
Contributor I

Thank you Thomas.

0 项奖励
回复
3,797 次查看
guoweisun
NXP TechSupport
NXP TechSupport

The termination resistor determined by the VCCA/VCCB setting,what're value of them in your side?

0 项奖励
回复
3,783 次查看
sd23
Contributor I

Both are 3.3V.

0 项奖励
回复