Network Layer protocol support in MQX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Network Layer protocol support in MQX

1,263 Views
PranayJoshi
Contributor I

Hello,

We want to communicate with the cloud using a WiFi module in one of the controllers which can have MQX RTOS

The communication between cloud and WiFi device should be secure using the below authentication and encryption protocols for 802.11 Wireless LAN access:

- EAP-TLS
-WPA2-PSK with passphrase
-PEAP/MSCHAPv2
-EAP-TTLS/PAP
-EAP-TTLS/MSCHAPv2
- CBC-MAC Protocol - (AES-CCMP)
 
Is MQX having the support of the above Network Layer protocols? 
Tags (1)
0 Kudos
Reply
1 Reply

1,210 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @PranayJoshi 

 

I would suggest you contact NXP's partner: Embedded Access for your question.  Embedded Access is the owner of MQX now.

http://embedded-access.com/

 

Regards

Daniel

0 Kudos
Reply