Network Layer protocol support in MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Network Layer protocol support in MQX

1,258 次查看
PranayJoshi
Contributor I

Hello,

We want to communicate with the cloud using a WiFi module in one of the controllers which can have MQX RTOS

The communication between cloud and WiFi device should be secure using the below authentication and encryption protocols for 802.11 Wireless LAN access:

- EAP-TLS
-WPA2-PSK with passphrase
-PEAP/MSCHAPv2
-EAP-TTLS/PAP
-EAP-TTLS/MSCHAPv2
- CBC-MAC Protocol - (AES-CCMP)
 
Is MQX having the support of the above Network Layer protocols? 
标记 (1)
0 项奖励
回复
1 回复

1,205 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi @PranayJoshi 

 

I would suggest you contact NXP's partner: Embedded Access for your question.  Embedded Access is the owner of MQX now.

http://embedded-access.com/

 

Regards

Daniel

0 项奖励
回复