Network Layer protocol support in MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Network Layer protocol support in MQX

1,262件の閲覧回数
PranayJoshi
Contributor I

Hello,

We want to communicate with the cloud using a WiFi module in one of the controllers which can have MQX RTOS

The communication between cloud and WiFi device should be secure using the below authentication and encryption protocols for 802.11 Wireless LAN access:

- EAP-TLS
-WPA2-PSK with passphrase
-PEAP/MSCHAPv2
-EAP-TTLS/PAP
-EAP-TTLS/MSCHAPv2
- CBC-MAC Protocol - (AES-CCMP)
 
Is MQX having the support of the above Network Layer protocols? 
タグ(1)
0 件の賞賛
返信
1 返信

1,209件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @PranayJoshi 

 

I would suggest you contact NXP's partner: Embedded Access for your question.  Embedded Access is the owner of MQX now.

http://embedded-access.com/

 

Regards

Daniel

0 件の賞賛
返信