MPC5744P Interrupt controller - TIMER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P Interrupt controller - TIMER

Jump to solution
5,770 Views
Veber
Contributor II

Hi,
I am working on Interrupt control monitor and there are three IRQs that are monitored. The monitor mode is set to EOI (see the attached picture). In that mode if IRQ latency exceeds that is set in LAT register, error should be signaled, but in the whole reference manual it doesn't says where it will be signaled. Can someone help me with this?

In my case if the IRQ exceeds the latency then INTC_MONITOR0 in FCCU resets my board, even though I set register to no reset reaction.

So if someone can explain me where will the error be signaled I would be very thankful.

0 Kudos
Reply
1 Solution
5,742 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, I am referring to this

Enabling of any fault reaction enables FOSU counter. You just need to clear the fault before ALARM period expires.

Pay attention to following appnote:

https://www.nxp.com/docs/en/application-note/AN5284.pdf

 

View solution in original post

0 Kudos
Reply
5 Replies
5,752 Views
Veber
Contributor II

Are you referring to this?


INTC2.PNG

Anyway after reading your comment, I disabled all FCCU faults and only enabled INTC_MONITOR0, inserted timeout error on IRQ_0 and board is still resetting...

0 Kudos
Reply
5,743 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, I am referring to this

Enabling of any fault reaction enables FOSU counter. You just need to clear the fault before ALARM period expires.

Pay attention to following appnote:

https://www.nxp.com/docs/en/application-note/AN5284.pdf

 

0 Kudos
Reply
5,690 Views
Veber
Contributor II

Thank you. The problem is solved!

0 Kudos
Reply
5,762 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it goes over FCCU. If you don't have enabled reset reaction to this fault, but you have enabled another one, it means also FOSU is active and it may reset the device if FCCU interrupt is not handled on time. Have you checked MC_RGM_DES? F_FFRR indicated FOSU reset.

davidtosenovjan_0-1655275979823.png

 

0 Kudos
Reply
5,760 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

In the past I made example for FOSU fault injection, but on different MCU that does not have RGM module. But FCCU works more or less same way.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-FCCU-FOSU-error-injection-GHS71...

 

0 Kudos
Reply