MMRF5014H

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMRF5014H

1,205 Views
jeffreyramos
Contributor I

Do you have installation and rework instructions for MMRF5014H?

0 Kudos
Reply
1 Reply

1,138 Views
LPP
NXP Employee
NXP Employee

Please, refer to this application note:

Solder Reflow Attach Method for High Power RF Devices in Air Cavity Packages

https://cache.nxp.com/docs/en/application-note/AN1908.pdf 


Have a great day,
Pavel
NXP TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply