MFRC631 TX optimization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFRC631 TX optimization

1,943件の閲覧回数
Taka1
Contributor I

I'm looking for a reference information for an MFRC631 to optimize TX behavior. There are some to change as follow.

8.6.2.1 set_residual_carrier bits

Table 126. TxAmp bits

Table 129. Txl register

Any register to modify the timing of Pch/Nch & Non Monotonic? 

As anohter example, for PN5180, there are some register related to MOD_FALLING/RISING. I'm expecting similar one.

0 件の賞賛
返信
3 返答(返信)

1,929件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

For the optimize TX of rc631 please refer to the 4.3 Optimizing the transmitting of the application note 

URL:https://www.nxp.com.cn/docs/en/application-note/AN11019.pdf.

You will find the information how to  optimize the transmitting. 

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信

1,925件の閲覧回数
Taka1
Contributor I

Thanks for explanation. Reached at what I expected. One minor further question. How can we modify Tr/Tf?

On AN11019.pdf, I could find "Tx Shaping (rise and fall time, if needed)". But couldn't find it & its similar one on MFRC631 datasheet. By any chance, TxClkMode is the one to modify? If you could give a hint, I'd appreciate it.

0 件の賞賛
返信

1,907件の閲覧回数
Taka1
Contributor I

Dear Fangfang,

Any update/clue? If you could guide me, I'd appreciate it.

0 件の賞賛
返信