Dear NXP..
Hi I'm now in a problematic situation. When I tried to run 'Start_TestTxRx' in NCJ29D5 SDK TestTxRx - v2.3.0 folder using Python, It says "could not open port 'COM42' : FileNotFoundError(2, 'no designated file.' , None, 2) I attached the picture for you.
It was fine until I flashed NCJ29D5_FlashAll.cmm and configured NCJ29D5 boards using GUI(file name is 'Evaluation tool')
please help TY
Hello @yjlee99 ,
I am sorry , but this is support channel for mass market products, you have to contact your assigned DFAE for further support on this.
Thanks for your patience and understanding!
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------