MCUXPRESSO IDE draw data series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXPRESSO IDE draw data series

Jump to solution
2,323 Views
LuigiV
Contributor III

In the MCUXpresso IDE, is there a way to draw in a window a data series ?

For example draw the content of an array graphically.

Luigi

0 Kudos
Reply
1 Solution
2,319 Views
donald795
Contributor I

Yes,

in MCUXpresso IDE, you can visualize a data series using the Peripherals+ view, Data Watchpoints and Tracing (DWT), or the FreeRTOS plugin for monitoring runtime data. For plotting, you can export Official Site data to a CSV file and use external tools like Excel or Python (with Matplotlib) to create the plot. This allows for flexible visualization of your data.

View solution in original post

0 Kudos
Reply
2 Replies
2,277 Views
brendonslade
NXP TechSupport
NXP TechSupport

You can also use FreeMASTER to plot data very easily. It has built in data plotting.

0 Kudos
Reply
2,320 Views
donald795
Contributor I

Yes,

in MCUXpresso IDE, you can visualize a data series using the Peripherals+ view, Data Watchpoints and Tracing (DWT), or the FreeRTOS plugin for monitoring runtime data. For plotting, you can export Official Site data to a CSV file and use external tools like Excel or Python (with Matplotlib) to create the plot. This allows for flexible visualization of your data.

0 Kudos
Reply