MC1322X programmer in a production context

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC1322X programmer in a production context

ソリューションへジャンプ
1,921件の閲覧回数
Houarcheneger
Contributor I

Hi everybody.

 

I developped a programm for an MC13224 with IAR embedded workbench. Now I would like to give the programm to the production department. For this I would need a flash programmer (only the software since I have got a J-Link). Could someone give some names ?

 

Thanks in advance.

 

Houarcheneger.

0 件の賞賛
返信
1 解決策
1,290件の閲覧回数
redbee
Contributor III

Over UART1,y ou can use flasher.c with mc1322x-load.pl to flash and image to the mc13224v:

 

http://mc1322x.devl.org/libmc1322x.html

 

you can also use Test_Tool and freescale's secondstage flash loader.

 

-Mar.

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,291件の閲覧回数
redbee
Contributor III

Over UART1,y ou can use flasher.c with mc1322x-load.pl to flash and image to the mc13224v:

 

http://mc1322x.devl.org/libmc1322x.html

 

you can also use Test_Tool and freescale's secondstage flash loader.

 

-Mar.

 

 

0 件の賞賛
返信
1,290件の閲覧回数
Houarcheneger
Contributor I

Ok thanks for your answer !

 

Do you know if I can use the JTAG port instead of UART1 ?

0 件の賞賛
返信