MC1322X programmer in a production context

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC1322X programmer in a production context

跳至解决方案
1,938 次查看
Houarcheneger
Contributor I

Hi everybody.

 

I developped a programm for an MC13224 with IAR embedded workbench. Now I would like to give the programm to the production department. For this I would need a flash programmer (only the software since I have got a J-Link). Could someone give some names ?

 

Thanks in advance.

 

Houarcheneger.

0 项奖励
回复
1 解答
1,307 次查看
redbee
Contributor III

Over UART1,y ou can use flasher.c with mc1322x-load.pl to flash and image to the mc13224v:

 

http://mc1322x.devl.org/libmc1322x.html

 

you can also use Test_Tool and freescale's secondstage flash loader.

 

-Mar.

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,308 次查看
redbee
Contributor III

Over UART1,y ou can use flasher.c with mc1322x-load.pl to flash and image to the mc13224v:

 

http://mc1322x.devl.org/libmc1322x.html

 

you can also use Test_Tool and freescale's secondstage flash loader.

 

-Mar.

 

 

0 项奖励
回复
1,307 次查看
Houarcheneger
Contributor I

Ok thanks for your answer !

 

Do you know if I can use the JTAG port instead of UART1 ?

0 项奖励
回复