LS1046A thermal design

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1046A thermal design

跳至解决方案
1,715 次查看
Nareshvarikuntla
Contributor III

Dear NXP,

I would like to have custom made heat sink attached to LS1046A. What is the maximum pressure LS1046A can able to withstand. How much contact pressure LS1046A needed for good thermal design.

I will be happy if you can share other relevant thermal design information.

Regards,

Naresh V.

标记 (2)
0 项奖励
回复
1 解答
1,704 次查看
Nareshvarikuntla
Contributor III

Thanks for the response.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,705 次查看
Nareshvarikuntla
Contributor III

Thanks for the response.

0 项奖励
回复
1,708 次查看
andrei_skok
NXP Employee
NXP Employee

Please look at the LS1046 Datasheet https://www.nxp.com/docs/en/data-sheet/LS1046A.pdf, chapter 6.3 Thermal management information.

Here you can find our recommendations for thermal design.

"The heat sink should be attached to the printed-circuit board with the spring force centered over the die. This spring force should not exceed 15 pounds force (65 N)."

0 项奖励
回复