LS1046A thermal design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A thermal design

ソリューションへジャンプ
1,713件の閲覧回数
Nareshvarikuntla
Contributor III

Dear NXP,

I would like to have custom made heat sink attached to LS1046A. What is the maximum pressure LS1046A can able to withstand. How much contact pressure LS1046A needed for good thermal design.

I will be happy if you can share other relevant thermal design information.

Regards,

Naresh V.

タグ(2)
0 件の賞賛
返信
1 解決策
1,702件の閲覧回数
Nareshvarikuntla
Contributor III

Thanks for the response.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,703件の閲覧回数
Nareshvarikuntla
Contributor III

Thanks for the response.

0 件の賞賛
返信
1,706件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

Please look at the LS1046 Datasheet https://www.nxp.com/docs/en/data-sheet/LS1046A.pdf, chapter 6.3 Thermal management information.

Here you can find our recommendations for thermal design.

"The heat sink should be attached to the printed-circuit board with the spring force centered over the die. This spring force should not exceed 15 pounds force (65 N)."

0 件の賞賛
返信