LS1028 board cannot support the std802.1CB-2017version?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028 board cannot support the std802.1CB-2017version?

3,648件の閲覧回数
xuchegndi
Contributor II

I cannot find any descriptions about the version std802.1CB in LS1028 ARM datasheet.

by testing redundant, I found that the R-tag only has 4 Bytes in LS1028, but in std802.1CB-2017, the R-tag has 6 Bytes.

it seems that LS1028 board cannot support the std802.1CB-2017version?

 

xuchegndi_0-1644808531117.png

 

タグ(2)
0 件の賞賛
返信
5 返答(返信)

3,641件の閲覧回数
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

The LS1028A switch was implemented against a pre-standard version 802.1CB-d2-2 (draft 2-2).

RED_TAG is a key area that changed when the spec was ratified.

0 件の賞賛
返信

3,634件の閲覧回数
xuchegndi
Contributor II

thanks for your reply.

so can I implement the 802.1 CB-2017 by upgrading firmware?

still, I do not know which version does LS1028A support for TSN serials like Qci, Qbv, Qbu, As, can you conform these versions for me? I can not find any version messages in data sheet. thanks

0 件の賞賛
返信

3,626件の閲覧回数
ufedor
NXP Employee
NXP Employee

> can I implement the 802.1 CB-2017 by upgrading firmware?

This is not possible because 4-byte RED_TAG is a hardware limitation.

> which version does LS1028A support for TSN serials like Qci, Qbv, Qbu

IEEE802.1Qci/D2.1

IEEE802.1Qbv/D3.1

IEEE 802.1Qbu/D3.0

Refer to the QorIQ LS1028A Reference Manual, 16.4 TSN-Capable Ethernet Switch.

0 件の賞賛
返信

3,619件の閲覧回数
xuchegndi
Contributor II

Thank you so much. 

is there any other NXP platforms which can support publish version (not draft version) of TSN serials? such as 802.1CB-2017 and 802.1QBV-2015 

タグ(1)
0 件の賞賛
返信

3,614件の閲覧回数
ufedor
NXP Employee
NXP Employee

> is there any other NXP platforms which can support publish version (not draft version) of TSN serials?

Currently - no.

0 件の賞賛
返信