Hi,
our customer want to get what is difference between UJA1169TK/3 and UJA1169TK/3Z.
can they PIN to PIN, would you like kindly help to share your comments.thanks.
Figure1: the datasheet shows the part number is UJA1169TK/3, it is not include UJA1169TK/3Z.
Figure 2: it shows UJA1169TK/3Z
Best regards.
Guofred
Solved! Go to Solution.
Hi Guofred,
The “Z” is not part of the type name, it is in the orderable part, showing the packing method for this product: Reel 13" Q1/T1 in Sulfur Barrier Bag.
In other words, the UJA1169TK/3 is the type name and the UJA1169TK/3Z is the ordering part number.
Best regards,
Tomas
Hi Guofred,
The “Z” is not part of the type name, it is in the orderable part, showing the packing method for this product: Reel 13" Q1/T1 in Sulfur Barrier Bag.
In other words, the UJA1169TK/3 is the type name and the UJA1169TK/3Z is the ordering part number.
Best regards,
Tomas