LS1028 board cannot support the std802.1CB-2017version?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028 board cannot support the std802.1CB-2017version?

1,724 Views
xuchegndi
Contributor II

I cannot find any descriptions about the version std802.1CB in LS1028 ARM datasheet.

by testing redundant, I found that the R-tag only has 4 Bytes in LS1028, but in std802.1CB-2017, the R-tag has 6 Bytes.

it seems that LS1028 board cannot support the std802.1CB-2017version?

 

xuchegndi_0-1644808531117.png

 

Tags (2)
0 Kudos
Reply
5 Replies

1,717 Views
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

The LS1028A switch was implemented against a pre-standard version 802.1CB-d2-2 (draft 2-2).

RED_TAG is a key area that changed when the spec was ratified.

0 Kudos
Reply

1,710 Views
xuchegndi
Contributor II

thanks for your reply.

so can I implement the 802.1 CB-2017 by upgrading firmware?

still, I do not know which version does LS1028A support for TSN serials like Qci, Qbv, Qbu, As, can you conform these versions for me? I can not find any version messages in data sheet. thanks

0 Kudos
Reply

1,702 Views
ufedor
NXP Employee
NXP Employee

> can I implement the 802.1 CB-2017 by upgrading firmware?

This is not possible because 4-byte RED_TAG is a hardware limitation.

> which version does LS1028A support for TSN serials like Qci, Qbv, Qbu

IEEE802.1Qci/D2.1

IEEE802.1Qbv/D3.1

IEEE 802.1Qbu/D3.0

Refer to the QorIQ LS1028A Reference Manual, 16.4 TSN-Capable Ethernet Switch.

0 Kudos
Reply

1,695 Views
xuchegndi
Contributor II

Thank you so much. 

is there any other NXP platforms which can support publish version (not draft version) of TSN serials? such as 802.1CB-2017 and 802.1QBV-2015 

Tags (1)
0 Kudos
Reply

1,690 Views
ufedor
NXP Employee
NXP Employee

> is there any other NXP platforms which can support publish version (not draft version) of TSN serials?

Currently - no.

0 Kudos
Reply