LS1023/43 USB VBUS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,230件の閲覧回数
fabio_sponticci
Contributor I

Hi,

I'm testing our prototypes and I found the step-up (3V3 to 5V) I'm using to provide the USB[1,2,3]_VBUS, is quite noisy. See attached picture.

So far I have no issue on the USB links but I have not started to stress the interfaces yet. 

Even if I'm inside the tolerance I would like to understand if the ac component could be an issue, and if I have to change the dcdc. 

Regards

Fabio

タグ(3)
0 件の賞賛
返信
1 解決策
3,224件の閲覧回数
ufedor
NXP Employee
NXP Employee

Something is really wrong with the 5V converter.

Please consult with the device manufacturer support.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,225件の閲覧回数
ufedor
NXP Employee
NXP Employee

Something is really wrong with the 5V converter.

Please consult with the device manufacturer support.

0 件の賞賛
返信
3,211件の閲覧回数
fabio_sponticci
Contributor I

Thanks, I'm aware of that and I'm working on that side too, therefore you're suggesting to improve it.

Have a good day

0 件の賞賛
返信