LS1023/43 USB VBUS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1023/43 USB VBUS

跳至解决方案
3,165 次查看
fabio_sponticci
Contributor I

Hi,

I'm testing our prototypes and I found the step-up (3V3 to 5V) I'm using to provide the USB[1,2,3]_VBUS, is quite noisy. See attached picture.

So far I have no issue on the USB links but I have not started to stress the interfaces yet. 

Even if I'm inside the tolerance I would like to understand if the ac component could be an issue, and if I have to change the dcdc. 

Regards

Fabio

标记 (3)
0 项奖励
回复
1 解答
3,159 次查看
ufedor
NXP Employee
NXP Employee

Something is really wrong with the 5V converter.

Please consult with the device manufacturer support.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,160 次查看
ufedor
NXP Employee
NXP Employee

Something is really wrong with the 5V converter.

Please consult with the device manufacturer support.

0 项奖励
回复
3,146 次查看
fabio_sponticci
Contributor I

Thanks, I'm aware of that and I'm working on that side too, therefore you're suggesting to improve it.

Have a good day

0 项奖励
回复