LS1023/43 USB VBUS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1023/43 USB VBUS

Jump to solution
1,123 Views
fabio_sponticci
Contributor I

Hi,

I'm testing our prototypes and I found the step-up (3V3 to 5V) I'm using to provide the USB[1,2,3]_VBUS, is quite noisy. See attached picture.

So far I have no issue on the USB links but I have not started to stress the interfaces yet. 

Even if I'm inside the tolerance I would like to understand if the ac component could be an issue, and if I have to change the dcdc. 

Regards

Fabio

Tags (3)
0 Kudos
Reply
1 Solution
1,117 Views
ufedor
NXP Employee
NXP Employee

Something is really wrong with the 5V converter.

Please consult with the device manufacturer support.

View solution in original post

0 Kudos
Reply
2 Replies
1,118 Views
ufedor
NXP Employee
NXP Employee

Something is really wrong with the 5V converter.

Please consult with the device manufacturer support.

0 Kudos
Reply
1,104 Views
fabio_sponticci
Contributor I

Thanks, I'm aware of that and I'm working on that side too, therefore you're suggesting to improve it.

Have a good day

0 Kudos
Reply