LQFP-48 marking code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,199件の閲覧回数
GBKK
Contributor I

Hello All, 

I've got a board with NXP microcontroller marked with following three lines of characters, but I'm not able to get back to NXP part number: is someone able to help me please ?

Are there some general NXP marking specifications or database for which it would be easy to get part numbers from marking codes ?

Marking on the chip is as follows:

S912

ZVCA96M

CTULYA

Thanks

0 件の賞賛
返信
1 解決策
3,187件の閲覧回数
GBKK
Contributor I

Great! 
That helps a lot!
Unfortunately I've got  no pictures with sufficient resolution of the chip (just looked at it with a no-photo capability microscope), but after a check on ref. manual  of MC9S12ZVC family,  I think  that p/n  is as follows:
S912ZVCA96F0MLFR
Thanks!

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,188件の閲覧回数
GBKK
Contributor I

Great! 
That helps a lot!
Unfortunately I've got  no pictures with sufficient resolution of the chip (just looked at it with a no-photo capability microscope), but after a check on ref. manual  of MC9S12ZVC family,  I think  that p/n  is as follows:
S912ZVCA96F0MLFR
Thanks!

Regards

0 件の賞賛
返信
3,192件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

The part number is sometimes adjusted at the package because of printing and size possibilities.

It could be this device - S912ZVCA96F0MLF, but I missing something. Could you please share a photo of the device?

Best regards,

Ladislav

0 件の賞賛
返信