LQFP-48 marking code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LQFP-48 marking code

跳至解决方案
3,208 次查看
GBKK
Contributor I

Hello All, 

I've got a board with NXP microcontroller marked with following three lines of characters, but I'm not able to get back to NXP part number: is someone able to help me please ?

Are there some general NXP marking specifications or database for which it would be easy to get part numbers from marking codes ?

Marking on the chip is as follows:

S912

ZVCA96M

CTULYA

Thanks

0 项奖励
回复
1 解答
3,196 次查看
GBKK
Contributor I

Great! 
That helps a lot!
Unfortunately I've got  no pictures with sufficient resolution of the chip (just looked at it with a no-photo capability microscope), but after a check on ref. manual  of MC9S12ZVC family,  I think  that p/n  is as follows:
S912ZVCA96F0MLFR
Thanks!

Regards

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,197 次查看
GBKK
Contributor I

Great! 
That helps a lot!
Unfortunately I've got  no pictures with sufficient resolution of the chip (just looked at it with a no-photo capability microscope), but after a check on ref. manual  of MC9S12ZVC family,  I think  that p/n  is as follows:
S912ZVCA96F0MLFR
Thanks!

Regards

0 项奖励
回复
3,201 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

The part number is sometimes adjusted at the package because of printing and size possibilities.

It could be this device - S912ZVCA96F0MLF, but I missing something. Could you please share a photo of the device?

Best regards,

Ladislav

0 项奖励
回复