LPC1769

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1769

1,840 次查看
syydmml
Contributor I

Neither j-link nor isp serial port can be used to burn lpc1769, and the circuit is normal. I changed the previous lpc1769 that can be burned to the circuit board, and it can be burned normally. I made 10 pieces of samples, and all the lpc769 above can not be burned normally.

0 项奖励
回复
4 回复数

1,828 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, could you tell me more about your setup, do you have the MCUXpresso? maybe you could try to do a mass erase. 

Pavel_Hernandez_0-1701390075455.png

Let me know if you need more help.

Best regards,
Pavel

0 项奖励
回复

1,819 次查看
syydmml
Contributor I

a825c65c6fa4a3b516fe3d7e6217865.pngadc6911f716a80a1d7c14591b69067e.png

These chips have been unable to connect successfully, does this mean that the chips are damaged? If not, is there any way to determine if the chip is damaged

0 项奖励
回复

1,812 次查看
syydmml
Contributor I

_20231201112422.jpg_20231201112557.jpg

Using isp serial port burning is also unable to connect successfully, and I found that the rx and tx pins are not voltage. I have a chip used before lpc1769 can be successfully connected, using isp and j-link can be

0 项奖励
回复

1,785 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I suggest reviewing the next information the TCK must need a pull-down.

Design Considerations for Debug - NXP Community

Best regards,
Pavel

0 项奖励
回复