LPC1769

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1769

1,828件の閲覧回数
syydmml
Contributor I

Neither j-link nor isp serial port can be used to burn lpc1769, and the circuit is normal. I changed the previous lpc1769 that can be burned to the circuit board, and it can be burned normally. I made 10 pieces of samples, and all the lpc769 above can not be burned normally.

0 件の賞賛
返信
4 返答(返信)

1,816件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, could you tell me more about your setup, do you have the MCUXpresso? maybe you could try to do a mass erase. 

Pavel_Hernandez_0-1701390075455.png

Let me know if you need more help.

Best regards,
Pavel

0 件の賞賛
返信

1,807件の閲覧回数
syydmml
Contributor I

a825c65c6fa4a3b516fe3d7e6217865.pngadc6911f716a80a1d7c14591b69067e.png

These chips have been unable to connect successfully, does this mean that the chips are damaged? If not, is there any way to determine if the chip is damaged

0 件の賞賛
返信

1,800件の閲覧回数
syydmml
Contributor I

_20231201112422.jpg_20231201112557.jpg

Using isp serial port burning is also unable to connect successfully, and I found that the rx and tx pins are not voltage. I have a chip used before lpc1769 can be successfully connected, using isp and j-link can be

0 件の賞賛
返信

1,773件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I suggest reviewing the next information the TCK must need a pull-down.

Design Considerations for Debug - NXP Community

Best regards,
Pavel

0 件の賞賛
返信