K32W041 API for DCDC module current?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32W041 API for DCDC module current?

2,588 Views
ckielstra
Contributor IV

We want to reduce the inrush current when waking up from sleep. 

Chapter 4.2.1 of the K32W041 User Manual (UM11323) states: “The configuration of the DCDC module can be optimized to suit the load current of the application; there are settings for 10 mA, 20 mA, 40 mA and 60 mA. The default configuration is 40 mA; software APIs are available to configure the other settings.”

Can someone point me to those software APIs?

0 Kudos
Reply
4 Replies

1,667 Views
MVWare
Contributor III

has this post been answered?  I need this info aswell

 

0 Kudos
Reply

1,425 Views
ckielstra
Contributor IV

I don't understand why @Ricardo_Zamora sent me a private reply, but his short reply was that he contacted the involved team. The DCDC trimming data is provisioned in the chip factory and that the customer should not modify the load current configurations. There are no related APIs for this configuration in the SDK.

This isn't exactly an answer to the question. We don't want to modify the trimming data, but we want to select one of the available power profiles. My follow-up question was never answered.

In a new electronics design we added a small choke coil to reduce the inrush peak.

0 Kudos
Reply

2,478 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

I apologize for the time spent on this. I sent you a private message.

 

Regards,

Ricardo

0 Kudos
Reply

2,550 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. I am checking your request.

As soon as I have some information to share, I will let you know!

 

Regards,

Ricardo