Is it possible to read multiple bytes of data at once from CLRC663's internal FIFO via RS232?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is it possible to read multiple bytes of data at once from CLRC663's internal FIFO via RS232?

679 次查看
Elly
Contributor I

Hello, 
There are 10 bytes of data read from tag memory in the internal FIFO(inventory).
Is there a way to read this data at once? 
Since the register for reading and writing FIFO data (0x05) is 1 byte, is there no choice but to read byte by byte?
The host interface is RS232. 

0 项奖励
回复
0 回复数