Initializing PCF8584T

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Initializing PCF8584T

1,255件の閲覧回数
madhanmani
Contributor I

Hello Sir/Madam,

I am working with PCF8584T and I could not initialize it,I tried all the flow chart information but can't communicate with it.Kindly suggest me to initialize and proceed further for Parallel to serial transfer.  

タグ(1)
0 件の賞賛
返信
1 返信

1,171件の閲覧回数
darioarias
NXP Employee
NXP Employee

Hello Madhan,

During the initialization did you consider the fact that the S0 and S0' registers are offset by one bit? This important because it means that if you program the own address register S0' with a value of 0x40, it will result in the value 0x80 being recognized as the PCF8584's slave address.

Darío

0 件の賞賛
返信