Initializing PCF8584T

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Initializing PCF8584T

1,262 Views
madhanmani
Contributor I

Hello Sir/Madam,

I am working with PCF8584T and I could not initialize it,I tried all the flow chart information but can't communicate with it.Kindly suggest me to initialize and proceed further for Parallel to serial transfer.  

Tags (1)
0 Kudos
Reply
1 Reply

1,178 Views
darioarias
NXP Employee
NXP Employee

Hello Madhan,

During the initialization did you consider the fact that the S0 and S0' registers are offset by one bit? This important because it means that if you program the own address register S0' with a value of 0x40, it will result in the value 0x80 being recognized as the PCF8584's slave address.

Darío

0 Kudos
Reply