(IW612/88W9098) Throughput is very low outside anechoic chamber under certain conditions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

(IW612/88W9098) Throughput is very low outside anechoic chamber under certain conditions

463 次查看
jun_1
Contributor IV

I am doing iperf test of IW612 and 88W9098. On both modules, throughput are very low outside anechoic chamber when they are configured to 802.11n/MCS7 on 5GHz circumstance; Please see the below for actual measured values.

Are there any possible wifi chipset side factors that may relate to this problem?

<iperf test result>

<802.11n/5GHz/MCS7>
anechoic chamber, distance 10m: 57Mbps
office, distance 1m: 58Mbps
office, distance 10m: 1.4Mbps

<802.11n/2.4GHz/MCS7>
anechoic chamber, distance 10m: 59Mbps
office, distance 1m: 46Mbps
office, distance 10m: 22Mbps

<802.11ax/2.4GHz/MCS7>
anechoic chamber, distance 10m: 75.5Mbps
office, distance 1m: 74.5Mbps
office, distance 10m: 68.7Mbps

→tested 2 IW612 modules, and both had similar results.

88W9098:
<802.11n/5GHz/MCS7/Spatial Streams:1>
anechoic chamber, distance 10m: no data
office, distance 1m :44.8Mbps
office, distance 10m: 7.3Mbps


============================================
〇Measurement environment:
iperf server/station: i.MX 8M Mini EVKB
wifi module:
murata/embeded artist, Type 1XL(Chipset: 88W9098)
murata/embeded artist, Type 2DL(Chipset: IW612)

adopter: Murata uSD-M2 adopter

〇WiFi chipset configulation:
using the following command to configure.
./mlanutl mlan1 txratecfg <1 for 802.11n, 3 for 802.11ax> <MCS value> 1

标签 (1)
  • RF

标记 (3)
0 项奖励
回复
0 回复数