ISP - <v4l2src0:pool0:src> can't allocate, setting maximum to minimum

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISP - <v4l2src0:pool0:src> can't allocate, setting maximum to minimum

ソリューションへジャンプ
644件の閲覧回数
r3gl0
Contributor II
Dear experts,
I'm currently working with the NXP IMX8MPLUS and trying to enable the ISP for the MT9V024 camera sensor.

My current set up is the following:

Yocto core image with IMAGE_INSTALL:append = " kernel-module-isp-vvcam gstreamer1.0 gstreamer1.0-plugins-base gstreamer1.0-plugins-good gstreamer1.0-plugins-bad v4l-utils isp-imx libtinyxml2 media-ctl fmt ".

Linux 5.15.71 Kirkstone
Is a headless build

Externally, I build in V4L2 mode:

- isp-imx-4.2.2.20.0
- isp-vvcam (lf-5.15.y_2.2.0)

My video convertor is telling me that there is video at 30 fps, width=752, height=480 on DPHY0
However, I cannot get a image from Gstreamer. I dont get any hard error, the closest thing is this information message: " <v4l2src0:pool0:src> can't allocate, setting maximum to minimum. "

Here is an example
root@imx8mp:~/build-out/sdk# gst-launch-1.0 -v v4l2src device=/dev/video0 num-buffers=5 ! "video/x-raw,format=YUY2,width=752,height=480,framerate=30/1" ! fakesink dump=true
0:00:00.000184125  2271   0x5599042800 INFO                GST_INIT gst.c:592:init_pre: Initializing GStreamer Core Library version 1.20.3
0:00:00.000278625  2271   0x5599042800 INFO                GST_INIT gst.c:593:init_pre: Using library installed in /usr/lib
0:00:00.000314500  2271   0x5599042800 INFO                GST_INIT gst.c:611:init_pre: Linux imx8mp 5.15.71+gea9b003902ee #1 SMP PREEMPT Tue Sep 12 14:15:41 UTC 2023 aarch64
0:00:00.000854500  2271   0x5599042800 INFO                GST_INIT gstmessage.c:129:_priv_gst_message_initialize: init messages
0:00:00.002470000  2271   0x5599042800 INFO                GST_INIT gstcontext.c:86:_priv_gst_context_initialize: init contexts
0:00:00.003066500  2271   0x5599042800 INFO      GST_PLUGIN_LOADING gstplugin.c:324:_priv_gst_plugin_initialize: registering 0 static plugins
0:00:00.003352750  2271   0x5599042800 INFO      GST_PLUGIN_LOADING gstplugin.c:232:gst_plugin_register_static: registered static plugin "staticelements"
0:00:00.003399125  2271   0x5599042800 INFO      GST_PLUGIN_LOADING gstplugin.c:234:gst_plugin_register_static: added static plugin "staticelements", result: 1
0:00:00.003510875  2271   0x5599042800 INFO            GST_REGISTRY gstregistry.c:1827:ensure_current_registry: reading registry cache: /home/root/.cache/gstreamer-1.0/registry.aarch64.bin
0:00:00.028175500  2271   0x5599042800 INFO            GST_REGISTRY gstregistrybinary.c:683:priv_gst_registry_binary_read_cache: loaded /home/root/.cache/gstreamer-1.0/registry.aarch64.bin in 0.024588 seconds
0:00:00.028346375  2271   0x5599042800 INFO            GST_REGISTRY gstregistry.c:1693:scan_and_update_registry: Validating plugins from registry cache: /home/root/.cache/gstreamer-1.0/registry.aarch64.bin
0:00:00.036117875  2271   0x5599042800 INFO            GST_REGISTRY gstregistry.c:1785:scan_and_update_registry: Registry cache has not changed
0:00:00.036177625  2271   0x5599042800 INFO            GST_REGISTRY gstregistry.c:1862:ensure_current_registry: registry reading and updating done, result = 1
0:00:00.036202250  2271   0x5599042800 INFO                GST_INIT gst.c:833:init_post: GLib runtime version: 2.72.3
0:00:00.036224750  2271   0x5599042800 INFO                GST_INIT gst.c:835:init_post: GLib headers version: 2.72.3
0:00:00.036241250  2271   0x5599042800 INFO                GST_INIT gst.c:837:init_post: initialized GStreamer successfully
0:00:00.036313000  2271   0x5599042800 INFO            GST_PIPELINE gstparse.c:344:gst_parse_launch_full: parsing pipeline description 'v4l2src device=/dev/video0 num-buffers=5 ! video/x-raw,format=YUY2,width=752,height=480,framerate=30/1 ! fakesink dump=true '
0:00:00.119030500  2271   0x5599042800 INFO      GST_PLUGIN_LOADING gstplugin.c:987:_priv_gst_plugin_load_file_for_registry: plugin "/usr/lib/gstreamer-1.0/libgstvideo4linux2.so" loaded
0:00:00.119095500  2271   0x5599042800 INFO     GST_ELEMENT_FACTORY gstelementfactory.c:489:gst_element_factory_create_with_properties: creating element "v4l2src"
0:00:00.125341875  2271   0x5599042800 INFO        GST_ELEMENT_PADS gstelement.c:759:gst_element_add_pad:<GstBaseSrc@0x55991ea130> adding pad 'src'
0:00:00.127313750  2271   0x5599042800 INFO      GST_PLUGIN_LOADING gstplugin.c:987:_priv_gst_plugin_load_file_for_registry: plugin "/usr/lib/gstreamer-1.0/libgstcoreelements.so" loaded
0:00:00.127381000  2271   0x5599042800 INFO     GST_ELEMENT_FACTORY gstelementfactory.c:489:gst_element_factory_create_with_properties: creating element "fakesink"
0:00:00.127746375  2271   0x5599042800 INFO        GST_ELEMENT_PADS gstelement.c:759:gst_element_add_pad:<GstBaseSink@0x55991e0610> adding pad 'sink'
0:00:00.127839250  2271   0x5599042800 INFO     GST_ELEMENT_FACTORY gstelementfactory.c:489:gst_element_factory_create_with_properties: creating element "pipeline"
0:00:00.128087000  2271   0x5599042800 INFO            GST_PIPELINE gst/parse/grammar.y:683:gst_parse_perform_link: linking some pad of GstV4l2Src named v4l2src0 to some pad of GstFakeSink named fakesink0 (0/0) with caps "video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1"
0:00:00.128130875  2271   0x5599042800 INFO     GST_ELEMENT_FACTORY gstelementfactory.c:489:gst_element_factory_create_with_properties: creating element "capsfilter"
0:00:00.128345250  2271   0x5599042800 INFO        GST_ELEMENT_PADS gstelement.c:759:gst_element_add_pad:<GstBaseTransform@0x55991f20e0> adding pad 'sink'
0:00:00.128396375  2271   0x5599042800 INFO        GST_ELEMENT_PADS gstelement.c:759:gst_element_add_pad:<GstBaseTransform@0x55991f20e0> adding pad 'src'
0:00:00.128437250  2271   0x5599042800 INFO              GST_STATES gstbin.c:2069:gst_bin_get_state_func:<pipeline0> getting state
0:00:00.128494250  2271   0x5599042800 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<capsfilter0> completed state change to NULL
0:00:00.128527625  2271   0x5599042800 INFO               GST_EVENT gstevent.c:1660:gst_event_new_reconfigure: creating reconfigure event
0:00:00.128564625  2271   0x5599042800 INFO        GST_ELEMENT_PADS gstutils.c:1816:gst_element_link_pads_full: trying to link element v4l2src0:(any) to element capsfilter0:sink
0:00:00.128592375  2271   0x5599042800 INFO        GST_ELEMENT_PADS gstelement.c:1016:gst_element_get_static_pad: found pad capsfilter0:sink
0:00:00.128618625  2271   0x5599042800 INFO                GST_PADS gstutils.c:1632:prepare_link_maybe_ghosting: v4l2src0 and capsfilter0 in same bin, no need for ghost pads
0:00:00.128662250  2271   0x5599042800 INFO                GST_PADS gstpad.c:2382:gst_pad_link_prepare: trying to link v4l2src0:src and capsfilter0:sink
0:00:00.128706250  2271   0x5599042800 INFO                GST_PADS gstpad.c:4357:gst_pad_peer_query:<capsfilter0:src> pad has no peer
0:00:00.128765750  2271   0x5599042800 INFO                GST_PADS gstpad.c:2590:gst_pad_link_full: linked v4l2src0:src and capsfilter0:sink, successful
0:00:00.128787375  2271   0x5599042800 INFO               GST_EVENT gstevent.c:1660:gst_event_new_reconfigure: creating reconfigure event
0:00:00.128810125  2271   0x5599042800 INFO               GST_EVENT gstpad.c:5946:gst_pad_send_event_unchecked:<v4l2src0:src> Received event on flushing pad. Discarding
0:00:00.128849500  2271   0x5599042800 INFO        GST_ELEMENT_PADS gstutils.c:1816:gst_element_link_pads_full: trying to link element capsfilter0:src to element fakesink0:(any)
0:00:00.128876375  2271   0x5599042800 INFO        GST_ELEMENT_PADS gstelement.c:1016:gst_element_get_static_pad: found pad capsfilter0:src
0:00:00.128907875  2271   0x5599042800 INFO                GST_PADS gstutils.c:1079:gst_pad_check_link: trying to link capsfilter0:src and fakesink0:sink
0:00:00.128978125  2271   0x5599042800 INFO                GST_PADS gstutils.c:1632:prepare_link_maybe_ghosting: capsfilter0 and fakesink0 in same bin, no need for ghost pads
0:00:00.129011625  2271   0x5599042800 INFO                GST_PADS gstpad.c:2382:gst_pad_link_prepare: trying to link capsfilter0:src and fakesink0:sink
0:00:00.129071250  2271   0x5599042800 INFO                GST_PADS gstpad.c:2590:gst_pad_link_full: linked capsfilter0:src and fakesink0:sink, successful
0:00:00.129091000  2271   0x5599042800 INFO               GST_EVENT gstevent.c:1660:gst_event_new_reconfigure: creating reconfigure event
0:00:00.129110625  2271   0x5599042800 INFO               GST_EVENT gstpad.c:5946:gst_pad_send_event_unchecked:<capsfilter0:src> Received event on flushing pad. Discarding
Setting pipeline to PAUSED ...
0:00:00.130531250  2271   0x5599042800 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<fakesink0> current NULL pending VOID_PENDING, desired next READY
0:00:00.130569250  2271   0x5599042800 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<fakesink0> completed state change to READY
0:00:00.130595000  2271   0x5599042800 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<fakesink0> notifying about state-changed NULL to READY (VOID_PENDING pending)
0:00:00.130650625  2271   0x5599042800 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'fakesink0' changed state to 2(READY) successfully
0:00:00.130682375  2271   0x5599042800 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<capsfilter0> current NULL pending VOID_PENDING, desired next READY
0:00:00.130707125  2271   0x5599042800 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<capsfilter0> completed state change to READY
0:00:00.130731875  2271   0x5599042800 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<capsfilter0> notifying about state-changed NULL to READY (VOID_PENDING pending)
0:00:00.130764125  2271   0x5599042800 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'capsfilter0' changed state to 2(READY) successfully
0:00:00.130796000  2271   0x5599042800 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<v4l2src0> current NULL pending VOID_PENDING, desired next READY
0:00:00.131003250  2271   0x5599042800 INFO                    v4l2 v4l2_calls.c:588:gst_v4l2_open:<v4l2src0:src> Opened device 'VIV' (/dev/video0) successfully
0:00:00.131045250  2271   0x5599042800 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<v4l2src0> completed state change to READY
0:00:00.131071625  2271   0x5599042800 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<v4l2src0> notifying about state-changed NULL to READY (VOID_PENDING pending)
0:00:00.131107625  2271   0x5599042800 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'v4l2src0' changed state to 2(READY) successfully
0:00:00.131145375  2271   0x5599042800 INFO              GST_STATES gstelement.c:2778:gst_element_continue_state:<pipeline0> committing state from NULL to READY, pending PAUSED, next PAUSED
0:00:00.131173500  2271   0x5599042800 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<pipeline0> notifying about state-changed NULL to READY (PAUSED pending)
0:00:00.131253250  2271   0x5599042800 INFO              GST_STATES gstelement.c:2786:gst_element_continue_state:<pipeline0> continue state change READY to PAUSED, final PAUSED
0:00:00.131305125  2271   0x5599042800 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<fakesink0> current READY pending VOID_PENDING, desired next PAUSED
0:00:00.131356500  2271   0x5599042800 INFO              GST_STATES gstbin.c:2935:gst_bin_change_state_func:<pipeline0> child 'fakesink0' is changing state asynchronously to PAUSED
0:00:00.131389875  2271   0x5599042800 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<capsfilter0> current READY pending VOID_PENDING, desired next PAUSED
0:00:00.131430000  2271   0x5599042800 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<capsfilter0> completed state change to PAUSED
0:00:00.131456875  2271   0x5599042800 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<capsfilter0> notifying about state-changed READY to PAUSED (VOID_PENDING pending)
0:00:00.131492250  2271   0x5599042800 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'capsfilter0' changed state to 3(PAUSED) successfully
0:00:00.131522125  2271   0x5599042800 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<v4l2src0> current READY pending VOID_PENDING, desired next PAUSED
0:00:00.131581625  2271   0x5599042800 INFO                 basesrc gstbasesrc.c:1430:gst_base_src_do_seek:<v4l2src0> seeking: time segment start=0:00:00.000000000, offset=0:00:00.000000000, stop=99:99:99.999999999, rate=1.000000, applied_rate=1.000000, flags=0x00, time=0:00:00.000000000, base=0:00:00.000000000, position 0:00:00.000000000, duration 99:99:99.999999999
0:00:00.131684250  2271   0x5599042800 INFO                    task gsttask.c:516:gst_task_set_lock: setting stream lock 0x55991ec260 on task 0x55991f4050
0:00:00.131710000  2271   0x5599042800 INFO                GST_PADS gstpad.c:6291:gst_pad_start_task:<v4l2src0:src> created task 0x55991f4050
0:00:00.131884375  2271   0x5599042800 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<v4l2src0> completed state change to PAUSED
0:00:00.131916375  2271   0x5599042800 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<v4l2src0> notifying about state-changed READY to PAUSED (VOID_PENDING pending)
0:00:00.131957500  2271   0x5599042800 INFO              GST_STATES gstbin.c:2971:gst_bin_change_state_func:<pipeline0> child 'v4l2src0' changed state to 3(PAUSED) successfully without preroll
0:00:00.131983625  2271   0x55991b3460 INFO        GST_ELEMENT_PADS gstelement.c:1013:gst_element_get_static_pad: no such pad 'sink' in element "v4l2src0"
0:00:00.131995000  2271   0x5599042800 INFO                pipeline gstpipeline.c:533:gst_pipeline_change_state:<pipeline0> pipeline is live
0:00:00.132039500  2271   0x5599042800 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<pipeline0> completed state change to PAUSED
0:00:00.132067875  2271   0x5599042800 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<pipeline0> notifying about state-changed READY to PAUSED (VOID_PENDING pending)
0:00:00.132120625  2271   0x55991b3460 INFO                 v4l2src gstv4l2src.c:550:gst_v4l2src_query_preferred_size:<v4l2src0> Detect input 0 as `camera`
Pipeline is live and does not need PREROLL ...
0:00:00.132187750  2271   0x55991b3460 INFO                    v4l2 gstv4l2object.c:1241:gst_v4l2_object_fill_format_list:<v4l2src0:src> got 4 format(s):
0:00:00.132220375  2271   0x55991b3460 INFO                    v4l2 gstv4l2object.c:1245:gst_v4l2_object_fill_format_list:<v4l2src0:src>   YUYV
0:00:00.132250750  2271   0x55991b3460 INFO                    v4l2 gstv4l2object.c:1245:gst_v4l2_object_fill_format_list:<v4l2src0:src>   NV12
0:00:00.132277000  2271   0x55991b3460 INFO                    v4l2 gstv4l2object.c:1245:gst_v4l2_object_fill_format_list:<v4l2src0:src>   NV16
0:00:00.132330375  2271   0x55991b3460 INFO                    v4l2 gstv4l2object.c:1245:gst_v4l2_object_fill_format_list:<v4l2src0:src>   BA10
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
0:00:00.133349250  2271   0x5599042800 INFO               GST_EVENT gstevent.c:1530:gst_event_new_latency: creating latency event 0:00:00.000000000
0:00:00.133414375  2271   0x5599042800 INFO                     bin gstbin.c:2759:gst_bin_do_latency_func:<pipeline0> configured latency of 0:00:00.000000000
0:00:00.133470250  2271   0x5599042800 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<fakesink0> current READY pending PAUSED, desired next PLAYING
0:00:00.133500625  2271   0x5599042800 INFO              GST_STATES gstbin.c:2935:gst_bin_change_state_func:<pipeline0> child 'fakesink0' is changing state asynchronously to PLAYING
0:00:00.133534000  2271   0x5599042800 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<capsfilter0> current PAUSED pending VOID_PENDING, desired next PLAYING
0:00:00.133564625  2271   0x5599042800 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<capsfilter0> completed state change to PLAYING
0:00:00.133592125  2271   0x5599042800 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<capsfilter0> notifying about state-changed PAUSED to PLAYING (VOID_PENDING pending)
0:00:00.133632125  2271   0x5599042800 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'capsfilter0' changed state to 4(PLAYING) successfully
0:00:00.133668750  2271   0x5599042800 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<v4l2src0> completed state change to PLAYING
0:00:00.133696625  2271   0x5599042800 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<v4l2src0> notifying about state-changed PAUSED to PLAYING (VOID_PENDING pending)
0:00:00.133766250  2271   0x5599042800 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'v4l2src0' changed state to 4(PLAYING) successfully
New clock: GstSystemClock
0:00:00.278604625  2271   0x55991b3460 INFO                    v4l2 gstv4l2object.c:4752:gst_v4l2_object_probe_caps:<v4l2src0:src> probed caps: video/x-raw, format=(string)YUY2, width=(int)[ 176, 4096, 16 ], height=(int)[ 144, 3072, 8 ], pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 30/1, 29/1, 28/1, 27/1, 26/1, 25/1, 24/1, 23/1, 22/1, 21/1, 20/1, 19/1, 18/1, 17/1, 16/1, 15/1, 14/1, 13/1, 12/1, 11/1, 10/1, 9/1, 8/1, 7/1, 6/1, 5/1, 4/1, 3/1, 2/1, 1/1 }; video/x-raw(format:Interlaced), format=(string)YUY2, width=(int)[ 176, 4096, 16 ], height=(int)[ 144, 3072, 8 ], pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 30/1, 29/1, 28/1, 27/1, 26/1, 25/1, 24/1, 23/1, 22/1, 21/1, 20/1, 19/1, 18/1, 17/1, 16/1, 15/1, 14/1, 13/1, 12/1, 11/1, 10/1, 9/1, 8/1, 7/1, 6/1, 5/1, 4/1, 3/1, 2/1, 1/1 }, interlace-mode=(string)alternate; video/x-raw, format=(string)NV12, width=(int)[ 176, 4096, 16 ], height=(int)[ 144, 3072, 8 ], pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 30/1, 29/1, 28/1, 27/1, 26/1, 25/1, 24/1, 23/1, 22/1, 21/1, 20/1, 19/1, 18/1, 17/1, 16/1, 15/1, 14/1, 13/1, 12/1, 11/1, 10/1, 9/1, 8/1, 7/1, 6/1, 5/1, 4/1, 3/1, 2/1, 1/1 }; video/x-raw(format:Interlaced), format=(string)NV12, width=(int)[ 176, 4096, 16 ], height=(int)[ 144, 3072, 8 ], pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 30/1, 29/1, 28/1, 27/1, 26/1, 25/1, 24/1, 23/1, 22/1, 21/1, 20/1, 19/1, 18/1, 17/1, 16/1, 15/1, 14/1, 13/1, 12/1, 11/1, 10/1, 9/1, 8/1, 7/1, 6/1, 5/1, 4/1, 3/1, 2/1, 1/1 }, interlace-mode=(string)alternate; video/x-raw, format=(string)NV16, width=(int)[ 176, 4096, 16 ], height=(int)[ 144, 3072, 8 ], pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 30/1, 29/1, 28/1, 27/1, 26/1, 25/1, 24/1, 23/1, 22/1, 21/1, 20/1, 19/1, 18/1, 17/1, 16/1, 15/1, 14/1, 13/1, 12/1, 11/1, 10/1, 9/1, 8/1, 7/1, 6/1, 5/1, 4/1, 3/1, 2/1, 1/1 }; video/x-raw(format:Interlaced), format=(string)NV16, width=(int)[ 176, 4096, 16 ], height=(int)[ 144, 3072, 8 ], pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 30/1, 29/1, 28/1, 27/1, 26/1, 25/1, 24/1, 23/1, 22/1, 21/1, 20/1, 19/1, 18/1, 17/1, 16/1, 15/1, 14/1, 13/1, 12/1, 11/1, 10/1, 9/1, 8/1, 7/1, 6/1, 5/1, 4/1, 3/1, 2/1, 1/1 }, interlace-mode=(string)alternate
0:00:00.290160875  2271   0x55991b3460 INFO                 v4l2src gstv4l2src.c:647:gst_v4l2src_negotiate:<v4l2src0> fixated to: video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
0:00:00.290237750  2271   0x55991b3460 INFO               GST_EVENT gstevent.c:892:gst_event_new_caps: creating caps event video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
0:00:00.290429750  2271   0x55991b3460 INFO           basetransform gstbasetransform.c:1325:gst_base_transform_setcaps:<capsfilter0> reuse caps
0:00:00.290487375  2271   0x55991b3460 INFO               GST_EVENT gstevent.c:892:gst_event_new_caps: creating caps event video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
/GstPipeline:pipeline0/GstV4l2Src:v4l2src0.GstPad:src: caps = video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
/GstPipeline:pipeline0/GstFakeSink:fakesink0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
0:00:00.406382625  2271   0x55991b3460 INFO                    v4l2 gstv4l2object.c:4083:gst_v4l2_object_set_format_full:<v4l2src0:src> Set capture framerate to 30/1
0:00:00.406454875  2271   0x55991b3460 INFO                    v4l2 gstv4l2object.c:3251:gst_v4l2_object_setup_pool:<v4l2src0:src> accessing buffers via mode 4
0:00:00.407197375  2271   0x55991b3460 INFO          v4l2bufferpool gstv4l2bufferpool.c:604:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool0:src> increasing minimum buffers to 2
0:00:00.407344250  2271   0x55991b3460 INFO          v4l2bufferpool gstv4l2bufferpool.c:617:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool0:src> reducing maximum buffers to 32
0:00:00.407469375  2271   0x55991b3460 INFO          v4l2bufferpool gstv4l2bufferpool.c:628:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool0:src> can't allocate, setting maximum to minimum
0:00:00.407735125  2271   0x55991b3460 INFO          v4l2bufferpool gstv4l2bufferpool.c:617:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool0:src> reducing maximum buffers to 32
0:00:00.407767625  2271   0x55991b3460 INFO          v4l2bufferpool gstv4l2bufferpool.c:628:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool0:src> can't allocate, setting maximum to minimum
0:00:00.420490625  2271   0x55991b3460 WARN          v4l2bufferpool gstv4l2bufferpool.c:884:gst_v4l2_buffer_pool_start:<v4l2src0:pool0:src> Uncertain or not enough buffers, enabling copy threshold

-------------------------------

I also tried gst-launch-1.0 -v  v4l2src device=/dev/video0 ! "video/x-raw,format=YUY2,width=752,height=480" ! queue ! videoconvert ! theoraenc ! oggmux ! filesink location=test_image.ogv , but i get a similar log.

Can anyone point me to the root of the issue?

------------------------------

My device tree looks like this:

&isp_0 {
    status = "okay";
};

&isp_1 {
    status = "disabled";
};

&dewarp {
    status = "okay";
};


&cameradev {
    status = "okay";
};

&isi_0 {
    status = "disabled";

    cap_device {
        status = "disabled";
    };

};

&isi_1 {
    status = "disabled";

    cap_device {
        status = "disabled";
    };
};

&mipi_csi_0 {
    status = "okay";

    port@0 {
        reg = <0>;
        mipi_csi0_ep: endpoint {
            remote-endpoint = <&mt9v024_mipi_0_ep>;
            data-lanes = <4>;
            csis-hs-settle = <16>;
        };
    };
};

-----
dmesg log:

[ 1740.645667] enter viv_dwe_exit_module
[ 1740.645797] enter dwe_hw_remove
[ 1740.645893] enter fake_pdev_release
[ 1740.645898] vvcam dewarp driver removed
[ 1740.665504] enter viv_isp_exit_module
[ 1740.665647] enter isp_hw_remove
[ 1740.665655] vvcam isp driver removed
[ 1740.701803] : Unregistered all entities
[ 1740.735600]
                MT9V024, r3gl0: probe
[ 1740.735611] enter mt9v024_probe
[ 1740.735621] xclk frequency: 24000000 Hz
[ 1740.735626]
                MT9V024, r3gl0 mt9v024_read_reg16: Reading reg=0x0000
[ 1740.749169] MT9V024, CHIP VERSION MATCH
[ 1740.749178]
                MT9V024, r3gl0: before after
[ 1740.749196] mt9v024_probe camera mipi mt9v024, is found
[ 1740.767059] enter viv_isp_init_module
[ 1740.767405] enter isp_hw_probe
[ 1740.767471] vvcam isp driver registered
[ 1740.778665] enter viv_dwe_init_module
[ 1740.778987] enter dwe_hw_probe
[ 1740.779312] vvcam dewarp driver probed
[ 1740.789973] enter viv_video_init_module
[ 1740.804690] imx8_media_dev: module is from the staging directory, the quality is unknown, you hav
e been warned.
[ 1740.805623] mx8-img-md: Registered sensor subdevice: mt9v024 2-0048 (1)
[ 1740.805644]
                MT9V024, r3gl0: Entering link_setup
[ 1740.805647]
                MT9V024, r3gl0: Entity name: mt9v024 2-0048
[ 1740.805649]
                MT9V024, r3gl0: Local pad index: 0, flags: 2
[ 1740.805653]
                MT9V024, r3gl0: Remote pad index: 0, flags: 1
[ 1740.805655]
                MT9V024, r3gl0: Link flags: 0
[ 1740.805658]
                MT9V024, r3gl0: Exiting link_setup
[ 1740.805660] mx8-img-md: created link [mt9v024 2-0048] => [mxc-mipi-csi2.0]
[ 1740.805666] mxc-md 32c00000.bus:camera: mxc_md_create_links
[ 1740.821137] enter isp_mi_stop
[ 1740.822206]
                MT9V024, r3gl0: mt9v024_enum_mbus_code
               
[ 1740.822218]
                MT9V024, r3gl0: mt9v024_get_format_code
               
[ 1740.822221]
                getting MEDIA_BUS_FMT_SGRBG10_1X10
[ 1740.823629]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=-2140645888
[ 1740.823647]
                MT9V024, r3gl0: mt9v024_query_capability
[ 1740.823650]
                MT9V024, r3gl0: mt9v024_query_capability + case
[ 1740.823652]
                MT9V024, r3gl0: returned mt9v024_query_capability
[ 1740.823655]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 1740.823658]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 1740.823660]
                flusher
[ 4323.157378]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=-2140645888
[ 4323.157391]
                MT9V024, r3gl0: mt9v024_query_capability
[ 4323.157395]
                MT9V024, r3gl0: mt9v024_query_capability + case
[ 4323.157397]
                MT9V024, r3gl0: returned mt9v024_query_capability
[ 4323.157399]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.157402]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.157404]
                flusher
[ 4323.169944] enter isp_mi_stop
[ 4323.233321]
                MT9V024, r3gl0: mt9v024_enum_mbus_code
               
[ 4323.233332]
                MT9V024, r3gl0: mt9v024_get_format_code
               
[ 4323.233336]
                getting MEDIA_BUS_FMT_SGRBG10_1X10
[ 4323.284807]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=-2140645888
[ 4323.284822]
                MT9V024, r3gl0: mt9v024_query_capability
[ 4323.284826]
                MT9V024, r3gl0: mt9v024_query_capability + case
[ 4323.284829]
                MT9V024, r3gl0: returned mt9v024_query_capability
[ 4323.284832]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.284835]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.284838]
                flusher
[ 4323.297599] enter isp_mi_stop
[ 4323.365311]
                MT9V024, r3gl0: mt9v024_enum_mbus_code
               
[ 4323.365321]
                MT9V024, r3gl0: mt9v024_get_format_code
               
[ 4323.365325]
                getting MEDIA_BUS_FMT_SGRBG10_1X10
[ 4323.444996]
                MT9V024, r3gl0: mt9v024_enum_mbus_code
               
[ 4323.445008]
                MT9V024, r3gl0: mt9v024_get_format_code
               
[ 4323.445012]
                getting MEDIA_BUS_FMT_SGRBG10_1X10
[ 4323.445045]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=-2140645888
[ 4323.445052]
                MT9V024, r3gl0: mt9v024_query_capability
[ 4323.445056]
                MT9V024, r3gl0: mt9v024_query_capability + case
[ 4323.445059]
                MT9V024, r3gl0: returned mt9v024_query_capability
[ 4323.445061]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.445065]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.445068]
                flusher
[ 4323.457682]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=261
[ 4323.457698]
                MT9V024, r3gl0: VVSENSORIOC_QUERY
[ 4323.457701]
                MT9V024, r3gl0: CONFIG_HARDENED_USERCOPY = 0
[ 4323.457704]
                MT9V024, r3gl0: mt9v024_query_supports
               
[ 4323.457707]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.457711]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.457713]
                flusher
[ 4323.626584]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=261
[ 4323.626602]
                MT9V024, r3gl0: VVSENSORIOC_QUERY
[ 4323.626604]
                MT9V024, r3gl0: CONFIG_HARDENED_USERCOPY = 0
[ 4323.626606]
                MT9V024, r3gl0: mt9v024_query_supports
               
[ 4323.626609]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.626612]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.626614]
                flusher
[ 4323.626627]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=257
[ 4323.626630]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.626632]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.626634]
                flusher
[ 4323.626638]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=260
[ 4323.626640]
                MT9V024, r3gl0 mt9v024_get_clk
[ 4323.626644]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.626646]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.626648]
                flusher
[ 4323.626652]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=259
[ 4323.626654]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.626657]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.626659]
                flusher
[ 4323.626662]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=256
[ 4323.626665]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.626667]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.626669]
                flusher
[ 4323.626672]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=262
[ 4323.626675]
                MT9V024, r3gl0: mt9v024_set_sensor_mode
               
[ 4323.626678]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.626681]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.626683]
                flusher
[ 4323.626686]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=263
[ 4323.626688]
                MT9V024, r3gl0: mt9v024_get_sensor_mode
               
[ 4323.626691]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.626693]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.626695]
                flusher
[ 4323.626701]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=261
[ 4323.626703]
                MT9V024, r3gl0: VVSENSORIOC_QUERY
[ 4323.626705]
                MT9V024, r3gl0: CONFIG_HARDENED_USERCOPY = 0
[ 4323.626707]
                MT9V024, r3gl0: mt9v024_query_supports
               
[ 4323.626709]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.626712]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.626714]
                flusher
[ 4323.639847] enter isp_mi_stop
[ 4323.642856]
                MT9V024, r3gl0: mt9v024_set_fmt
               
[ 4323.642866]
                MT9V024, r3gl0: mt9v024_get_format_code
               
[ 4323.642869]
                getting MEDIA_BUS_FMT_SGRBG10_1X10
[ 4323.642876]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=285
[ 4323.642881]
                MT9V024, r3gl0 mt9v024_set_test_pattern - NOT implemented
[ 4323.642883]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.642886]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.642888]
                flusher
[ 4323.642898]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=279
[ 4323.642901]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.642903]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.642905]
                flusher
[ 4323.642908]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=263
[ 4323.642911]
                MT9V024, r3gl0: mt9v024_get_sensor_mode
               
[ 4323.642913]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.642916]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.642918]
                flusher
[ 4323.643324]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=274
[ 4323.643332]
                MT9V024, r3gl0 mt9v024_set_exp - Not implemented
[ 4323.643335]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.643338]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.643340]
                flusher
[ 4323.643346]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=277
[ 4323.643348]
                MT9V024, r3gl0 mt9v024_set_gain - Not implemented
[ 4323.643350]
                MT9V024, r3gl0: mt9v024_priv_ioctl after case, ret=0
[ 4323.643353]
                MT9V024, r3gl0: mt9v024_priv_ioctl before final return
[ 4323.643355]
                flusher
[ 4323.645211]
                MT9V024, r3gl0: mt9v024_enum_mbus_code
               
[ 4323.645223]
                MT9V024, r3gl0: mt9v024_get_format_code
               
[ 4323.645226]
                getting MEDIA_BUS_FMT_SGRBG10_1X10
[ 4323.645342]
                MT9V024, r3gl0: mt9v024_enum_mbus_code
               
[ 4323.645345]
                MT9V024, r3gl0: mt9v024_get_format_code
               
[ 4323.645347]
                getting MEDIA_BUS_FMT_SGRBG10_1X10
[ 4323.645486] enter isp_s_comp
[ 4323.645500] enter isp_s_comp
[ 4323.645505] enter isp_s_comp
[ 4323.645605]
                MT9V024, r3gl0: mt9v024_enum_mbus_code
               
[ 4323.645608]
                MT9V024, r3gl0: mt9v024_get_format_code
               
[ 4323.645610]
                getting MEDIA_BUS_FMT_SGRBG10_1X10
[ 4323.661739] enter wdr3_hw_init
[ 4323.661752] wdr3 res: 752 480
[ 4323.693491] enter isp_set_stream 1
[ 4323.704723] enter isp_mi_start
[ 4323.705232]
                MT9V024, r3gl0: mt9v024_priv_ioctl request, cmd=272
[ 4323.705245]
                MT9V024, r3gl0: mt9v024_s_stream enable: 1  
[ 4323.705249]
                MT9V024, r3gl0: mt9v024_superinit
               
[ 4327.005171]  MT9V024, r3gl0: Sensor enabled

---
this is how my media looks like:

root@imx8mp:~/build-out/sdk# media-ctl -p -d /dev/media0
Media controller API version 5.15.71

Media device information
------------------------
driver          vvcam-video
model           viv_media
serial          
bus info        
hw revision     0x0
driver version  5.15.71

Device topology
- entity 1: viv_v4l20 (1 pad, 1 link)
            type Node subtype V4L flags 0
            device node name /dev/video0
        pad0: Sink
                <- "vvcam-dwe.0":0 [ENABLED]

- entity 5: vvcam-dwe.0 (2 pads, 2 links)
            type Node subtype V4L flags 0
            device node name /dev/v4l-subdev0
        pad0: Source
                -> "viv_v4l20":0 [ENABLED]
        pad1: Sink
                <- "vvcam-isp.0":0 [ENABLED]

- entity 8: vvcam-isp.0 (1 pad, 1 link)
            type Node subtype V4L flags 0
            device node name /dev/v4l-subdev1
        pad0: Source
                -> "vvcam-dwe.0":1 [ENABLED]

root@imx8mp:~/build-out/sdk# media-ctl -p -d /dev/media1
Media controller API version 5.15.71

Media device information
------------------------
driver          mxc-md
model           FSL Capture Media Device
serial          
bus info        
hw revision     0x0
driver version  5.15.71

Device topology
- entity 1: mxc-mipi-csi2.0 (8 pads, 1 link)
            type Node subtype V4L flags 0
            device node name /dev/v4l-subdev2
        pad0: Sink
                <- "mt9v024 2-0048":0 [ENABLED,IMMUTABLE]
        pad1: Sink
        pad2: Sink
        pad3: Sink
        pad4: Source
        pad5: Source
        pad6: Source
        pad7: Source

- entity 10: mt9v024 2-0048 (1 pad, 1 link)
             type V4L2 subdev subtype Sensor flags 0
             device node name /dev/v4l-subdev3
        pad0: Source
                [fmt:SGRBG10_1X10/752x480 field:none]
                -> "mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE]

----

my dewarp json file looks like this: 

{
"dewarpConfigArray" :[
{
"source_image":{
"width" : 752,
"height" : 480
},

"?dewarpType": "LENS_CORRECTION, FISHEYE_EXPAND, SPLIT_SCREEN",
"dewarpType": "FISHEYE_DEWARP",

"scale": {
"roix" : 0,
"roiy" : 0,
"factor" : 1.0
},

"split": {
"horizon_line" : 240,
"vertical_line_up" : 367,
"vertical_line_down": 367
},

"bypass" : true,
"hflip" : false,
"vflip" : false,

"camera_matrix" : [ 3.9177894938743270e+003, 0., 1.9716642989691159e+003, 0.,3.9177894938743270e+003, 1.1024451486734267e+003, 0., 0., 1. ],
"distortion_coeff": [ -1.3019040624278982e-001, 2.2621318183135611e-001,1.2109476203374344e-003, 9.4317229120640680e-004,-7.1053958306120402e-001 ],
"perspective" : [1.0, 0, 0, 0, 1, 0, 0, 0, 1]

}
]

}

タグ(3)
0 件の賞賛
返信
1 解決策
213件の閲覧回数
r3gl0
Contributor II
I had a hardware issue that did not allowed proper CSI communication.

Regarding adapting the 1920x1080 to 752x480, I can confirm it does not produce a correct image, but it will get you an output.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
543件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
458件の閲覧回数
r3gl0
Contributor II

Hi @Bio_TICFSL, I already checked this, but it's been hard to pinpoint the exact error

I have a theory: I created my calibration file by borrowing the OS08a20_8M_10_1080p_linear.xml file. I did change the sensor name and resolution strings to match my sensor, but I’m wondering if changing the resolution from 1920x1080 to 752x480 could be causing an issue with the ISP. I understand this wouldn’t produce a correct image, but at this point, I’m just trying to get any kind of signal image, even if it’s distorted or incorrect.

Is this likely the reason I’m not getting any output at all? Or should I still expect to get at least something even with an incorrect calibration?

If this is the issue, is there a way I can generate a basic/dummy 752x480 calibration file just to test and get some output? I’m not concerned about image quality right now, I am just looking for testing the pipeline.

0 件の賞賛
返信
214件の閲覧回数
r3gl0
Contributor II
I had a hardware issue that did not allowed proper CSI communication.

Regarding adapting the 1920x1080 to 752x480, I can confirm it does not produce a correct image, but it will get you an output.
0 件の賞賛
返信
462件の閲覧回数
r3gl0
Contributor II

I also built isp-imx in debug mode and tried the following:

root@imx8mp:~/build-out/sdk# gst-launch-1.0 -v v4l2src device=/dev/video0 ! "video/x-raw,format=YUY2,width=752,height=480,framerate=30/1" ! fakesink dump=true
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
/GstPipeline:pipeline0/GstV4l2Src:v4l2src0.GstPad:src: caps = video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
/GstPipeline:pipeline0/GstFakeSink:fakesink0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)752, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
INFO : [V4l2Event] Compose: left=0,top=0,width=752,height=480

INFO : [NativeSensor] jsonRequest 0xa01f
INFO : [MediaPipeline] MEDIA_EVENT_STREAM_OPEN
INFO : [MediaPipeline] stream0 connect NativeSensor:0 ---> NativeDewarp:0
INFO : [MediaPipeline] stream0 connect NativeDewarp:0 ---> V4l2Control:0
INFO : [MediaPipeline] MEDIA_EVENT_STREAM_SET_FMT
INFO : [MediaPipeline] set format:0 res: 752 480 1
INFO : [NativeSensor] setFormat isp crop: bounds 752X480 left 0 top 0 size 752X480

INFO : [NativeSensor] setFormat isp scale: bounds 752X480 left 0 top 0 size 752X480

[CITF][INF]: RESULT camdev::CitfDevice::calibrationLoadandInit(Json::Value&, Json::Value&)
[CITF][INF]: camdev::Operation::Operation(camdev::Operation_Handle*) (enter)
[CITF][INF]: camdev::SensorOps::SensorOps(camdev::CalibSensor&, HalHolder*) (enter)
[CITF][INF]: camdev::SensorOps::SensorOps(camdev::CalibSensor&, HalHolder*) (exit)
[CITF][INF]: camdev::SensorOps::SensorOps(camdev::CalibSensor&, HalHolder*) (enter)
[CITF][INF]: camdev::SensorOps::SensorOps(camdev::CalibSensor&, HalHolder*) (exit)
[CITF][INF]: camdev::SensorOps::SensorOps(camdev::CalibSensor&, HalHolder*) (enter)
[CITF][INF]: camdev::SensorOps::SensorOps(camdev::CalibSensor&, HalHolder*) (exit)
[CITF][INF]: camdev::SensorOps::SensorOps(camdev::CalibSensor&, HalHolder*) (enter)
[CITF][INF]: camdev::SensorOps::SensorOps(camdev::CalibSensor&, HalHolder*) (exit)
[CITF][INF]: camdev::Operation::Operation(camdev::Operation_Handle*) (exit)
[CITF][INF]: RESULT camdev::CitfSensor::sensorOpen(Json::Value&, Json::Value&)
CALIB_INF: tag: AF
CALIB_INF: tag: AEC
CALIB_WAN: Don't support: DampOverVideo
CALIB_WAN: Don't support: DampUnderVideo
CALIB_INF: tag: DEGAMMA
CALIB_INF: tag: WDR
[CITF][INF]: CitfBufferPoolClearBufList!, chain ID:0
[CITF][INF]: camdev::BuffPool* camdev::Bitf::bitfGetBufferPoolCtrl(ISPCORE_BUFIO_ID)
INFO : [MediaBufferQueue] create buffer queue 752 480 1 4
DEBUG : [MediaBuffer] alloc buffer 0x66c00000 0x000b1000
DEBUG : [MediaBuffer] alloc buffer 0x66d00000 0x000b1000
DEBUG : [MediaBuffer] alloc buffer 0x66f00000 0x000b1000
DEBUG : [MediaBuffer] alloc buffer 0x67000000 0x000b1000
INFO : [NativeSensor] push NativeDewarp sink buffer 0x66c00000 into isp
[CITF][INF]: CitfBufferPoolAddEntity!, chain ID:0
[CITF][INF]: camdev::BuffPool* camdev::Bitf::bitfGetBufferPoolCtrl(ISPCORE_BUFIO_ID)
[CITF][INF]: static RESULT camdev::Bitf::bitfCheckBufSizeMax(uint32_t, ISPCORE_BUFIO_ID)
INFO : [NativeSensor] push NativeDewarp sink buffer 0x66d00000 into isp
[CITF][INF]: CitfBufferPoolAddEntity!, chain ID:0
[CITF][INF]: camdev::BuffPool* camdev::Bitf::bitfGetBufferPoolCtrl(ISPCORE_BUFIO_ID)
[CITF][INF]: static RESULT camdev::Bitf::bitfCheckBufSizeMax(uint32_t, ISPCORE_BUFIO_ID)
INFO : [NativeSensor] push NativeDewarp sink buffer 0x66f00000 into isp
[CITF][INF]: CitfBufferPoolAddEntity!, chain ID:0
[CITF][INF]: camdev::BuffPool* camdev::Bitf::bitfGetBufferPoolCtrl(ISPCORE_BUFIO_ID)
[CITF][INF]: static RESULT camdev::Bitf::bitfCheckBufSizeMax(uint32_t, ISPCORE_BUFIO_ID)
INFO : [NativeSensor] push NativeDewarp sink buffer 0x67000000 into isp
[CITF][INF]: CitfBufferPoolAddEntity!, chain ID:0
[CITF][INF]: camdev::BuffPool* camdev::Bitf::bitfGetBufferPoolCtrl(ISPCORE_BUFIO_ID)
[CITF][INF]: static RESULT camdev::Bitf::bitfCheckBufSizeMax(uint32_t, ISPCORE_BUFIO_ID)
[CITF][INF]: CitfBufferPoolKernelAddrMap!, chain ID:0
[CITF][INF]: camdev::BuffPool* camdev::Bitf::bitfGetBufferPoolCtrl(ISPCORE_BUFIO_ID)
[CITF][INF]: CitfBufferPoolSetBufToEngine!, chain ID:0
[CITF][INF]: camdev::BuffPool* camdev::Bitf::bitfGetBufferPoolCtrl(ISPCORE_BUFIO_ID)
[CITF][INF]: CitfBufferPoolSetBufToEngine!, chain ID:0 buffer counter number , buf_context:4, set to Engine:4
[CITF][INF]: static RESULT camdev::Bitf::bitfCheckBufNumberMax(uint32_t, ISPCORE_BUFIO_ID)
[CITF][INF]: RESULT camdev::CitfDevice::cameraConnect(Json::Value&, Json::Value&)
[CITF][INF]: int32_t camdev::Operation::cameraConnect(bool, ItfBufferCb*, const ConnectInfo&) (enter)
CAMERIC-MI-DRV: CamerIcMiInit: (enter)
CAMERIC-MI-DRV: CamerIcMiInit: (exit)
CAMERIC-ISP-WDR-DRV: CamerIcIspWdr2Init: (enter)
CAMERIC-ISP-WDR-DRV: CamerIcIspWdr2Init: (exit)
[CITF][INF]: pathConfigSet in, set path, state: 0
[CITF][INF]: int32_t camdev::Operation::inputConnect() (enter)
CAMERIC-MI-DRV: CamerIcMiRegisterRequestCb: (enter)
CAMERIC-MI-DRV: CamerIcMiRegisterRequestCb: (exit)
CAMERIC-MI-DRV: CamerIcMiRegisterEventCb: (enter)
CAMERIC-MI-DRV: CamerIcMiRegisterEventCb: (exit)
CAMERIC-ISP-CAC-DRV: CamerIcIspCacDisable: (enter)
CAMERIC-ISP-CAC-DRV: CamerIcIspCacDisable: (exit)
CAMERIC-ISP-CAC-DRV: CamerIcIspCacConfig: (enter)
CAMERIC-ISP-CAC-DRV: CamerIcIspCacConfig: (exit)
CAMERIC-ISP-CAC-DRV: CamerIcIspCacEnable: (enter)
CAMERIC-ISP-CAC-DRV: CamerIcIspCacEnable: (exit)
CAMERIC-MI-DRV: CamerIcMiSetBurstLength: (enter)
CAMERIC-MI-DRV: CamerIcMiSetBurstLength: (exit)
CAMERIC-MI-DRV: CamerIcMiSetResolution: (enter)
CAMERIC-MI-DRV: CamerIcMiSetResolution: set resolution 0 (752, 480)->(752, 480)
CAMERIC-MI-DRV: CamerIcMiSetResolution: (exit)
CAMERIC-MI-DRV: CamerIcMiSetResolution: (enter)
CAMERIC-MI-DRV: CamerIcMiSetResolution: set resolution 1 (752, 480)->(752, 480)
CAMERIC-MI-DRV: CamerIcMiSetResolution: (exit)
CAMERIC-MI-DRV: CamerIcMiSetResolution: (enter)
CAMERIC-MI-DRV: CamerIcMiSetResolution: set resolution 2 (752, 480)->(752, 480)
CAMERIC-MI-DRV: CamerIcMiSetResolution: (exit)
CAMERIC-MI-DRV: CamerIcMiSetResolution: (enter)
CAMERIC-MI-DRV: CamerIcMiSetResolution: set resolution 3 (752, 480)->(752, 480)
CAMERIC-MI-DRV: CamerIcMiSetResolution: (exit)
CAMERIC-MI-DRV: CamerIcMiSetResolution: (enter)
CAMERIC-MI-DRV: CamerIcMiSetResolution: set resolution 4 (752, 480)->(752, 480)
CAMERIC-MI-DRV: CamerIcMiSetResolution: (exit)
CAMERIC-MI-DRV: CamerIcMiSetDataMode: (enter) 4
CAMERIC-MI-DRV: CamerIcMiSetDataMode: set datamode (0, 4)
CAMERIC-MI-DRV: CamerIcMiSetDataMode: (exit)
CAMERIC-MI-DRV: CamerIcMiSetDataLayout: (enter)
CAMERIC-MI-DRV: CamerIcMiSetDataLayout: set datalayout (0, 3)
CAMERIC-MI-DRV: CamerIcMiSetDataLayout: (exit)
CAMERIC-MI-DRV: CamerIcMiSetDataAlignMode: (enter) alignmode: 0, path:0
CAMERIC-MI-DRV: CamerIcMiSetDataAlignMode: set data_align_mode (0, 0)
CAMERIC-MI-DRV: CamerIcMiSetDataAlignMode: (exit)
CAMERIC-MI-DRV: CamerIcMiSetDataMode: (enter) 1
CAMERIC-MI-DRV: CamerIcMiSetDataMode: set datamode (1, 1)
CAMERIC-MI-DRV: CamerIcMiSetDataMode: (exit)
CAMERIC-MI-DRV: CamerIcMiSetDataLayout: (enter)
CAMERIC-MI-DRV: CamerIcMiSetDataLayout: set datalayout (1, 3)
CAMERIC-MI-DRV: CamerIcMiSetDataLayout: (exit)
CAMERIC-MI-DRV: CamerIcMiSetDataAlignMode: (enter) alignmode: 0, path:1
CAMERIC-MI-DRV: CamerIcMiSetDataAlignMode: set data_align_mode (1, 0)
CAMERIC-MI-DRV: CamerIcMiSetDataAlignMode: (exit)
CAMERIC-MI-DRV: CamerIcMiSetDataMode: (enter) 1
CAMERIC-MI-DRV: CamerIcMiSetDataMode: set datamode (2, 1)
CAMERIC-MI-DRV: CamerIcMiSetDataMode: (exit)
CAMERIC-MI-DRV: CamerIcMiSetDataLayout: (enter)
CAMERIC-MI-DRV: CamerIcMiSetDataLayout: set datalayout (2, 3)
CAMERIC-MI-DRV: CamerIcMiSetDataLayout: (exit)
CAMERIC-MI-DRV: CamerIcMiSetDataAlignMode: (enter) alignmode: 0, path:2
CAMERIC-MI-DRV: CamerIcMiSetDataAlignMode: set data_align_mode (2, 0)
CAMERIC-MI-DRV: CamerIcMiSetDataAlignMode: (exit)
[CITF][INF]: CAM_ENGINE_CMD_START, ret = 0x0
CAMERIC-ISP-CAC-DRV: CamerIcIspCacEnable: (enter)
CAMERIC-ISP-CAC-DRV: CamerIcIspCacEnable: (exit)
[CITF][INF]: int32_t camdev::Operation::inputConnect() (exit)
[CITF][INF]: int32_t camdev::Operation::cameraConnect(bool, ItfBufferCb*, const ConnectInfo&) (exit)
INFO : [NativeSensor] setFormat 1 752 480, type 1, port: 0
INFO : [NativeDewarp] setFormat 1 752 480, type 0, port: 0
INFO : [NativeDewarp] setFormat dewarp input: 752x480 YUV422I

INFO : [NativeDewarp] setFormat 1 752 480, type 1, port: 0
INFO : [NativeDewarp] setFormat dewarp output: 752x480 YUV422I

INFO : [V4l2Event] get json request: {"id":"s.fps","fps":30}
INFO : [NativeSensor] jsonRequest 0x1801a
INFO : [V4l2Event] send json response: {
"result" : 0
}

INFO : [MediaPipeline] MEDIA_EVENT_STREAM_START
INFO : [DewarpDriver] start 752 480 48 31, stride: 1504 1504
INFO : [DEWARP_HW] enter setParams
INFO : [NativeSensor] enter start
[CITF][INF]: RESULT camdev::CitfDevice::previewStart(Json::Value&, Json::Value&)
[CITF][INF]: int32_t camdev::Operation::previewStart() (enter)
[CITF][INF]: int32_t camdev::Operation::streamingStart(uint) (enter)
HAL-ALTERA: HalConnectIrq connect src: 0
HAL-ALTERA: HalConnectIrq connect src: 4
HAL-ALTERA: HalConnectIrq connect src: 1
HAL-ALTERA: HalConnectIrq connect src: 2
[CITF][INF]: CAM_ENGINE_CMD_START_STREAMING, ret = 0x0
[CITF][INF]: int32_t camdev::Operation::streamingStart(uint) (exit)
[CITF][INF]: int32_t camdev::Operation::previewStart() (exit)
[CITF][INF]: CitfInitOutChain!, chain ID:0, frame_skip:0
[CITF][INF]: camdev::Xom::Xom() (enter)
[CITF][INF]: camdev::Xom::Xom() (exit)
[CITF][INF]: camdev::Xom::Xom(ISPCORE_BUFIO_ID, uint32_t, uint32_t) (enter)
[CITF][INF]: camdev::Xom::Xom(ISPCORE_BUFIO_ID, uint32_t, uint32_t) (exit)
[CITF][INF]: RESULT camdev::Bitf::bitfSetOutputCtrl(ISPCORE_BUFIO_ID, camdev::Xom*)
[CITF][INF]: CitfStartOutChain!, chain ID:0
[CITF][INF]: CitfAttachChain!, chain ID:0

-------
root@imx8mp:~/build-out/sdk# ./vvext 0 "CAPTURE" 0
INFO : [VVEXT:] Open Device: /dev/video0 (fd=3)
INFO : [VVEXT:] Driver: viv_v4l2_device
INFO : [VVEXT:] found viv video dev /dev/video0
INFO : [V4l2Event] get json request: {
"id" : "dwe.g.params",
"streamid" : 0
}

INFO : [NativeSensor] jsonRequest 0x81000
INFO : [V4l2Event] send json response: {
"dwe" :
{
"bypass" : true,
"hflip" : false,
"mat" :
[
0.0,
0.0,
0.0,
0.0,
0.0,
0.0,
0.0,
0.0,
0.0,
0.0,
0.0,
0.0,
0.0,
0.0,
0.0,
0.0,
0.0
],
"mode" : 0,
"vflip" : false
},
"result" : 0
}

INFO : [VVEXT:] get command CAPTURE 0
INFO : [V4l2Event] get json request: {
"id" : "capture",
"streamid" : 0
}

INFO : [NativeSensor] jsonRequest 0x80002
ERROR : [NativeSensor] CaptureImage dump buf failed 1

INFO : [V4l2Event] send json response: {
"CaptureImage" : "Image_752_480_YUV422I_20220428175226.yuv",
"result" : -1
}

Capture Image_752_480_YUV422I_20220428175226.yuv failed


------------

Feels like ISP does not have any issue but when capturing the image. wwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwww

0 件の賞賛
返信