I2C write timeout for second time write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C write timeout for second time write

6,020 Views
shrithi
Contributor I

Hii  Support team,

We are using i. MX8QM processor. We are experiencing an issue with i2c write.
The first I2C write will pass, but there is a problem with the second I2C write.

Below error we are getting for second i2c write.

mipi_test 4-003d: write_reg: error -110: reg=b3b3, val=21
Error setting pattern and resolution: Connection timed out

Any configuration required in imx i2c master side?

I tried to write with i2cset command and it showing below message

Error: Could not set address to 0x3d: Device or resource busy

Can you please provide the suggestion to solve this error?

 

0 Kudos
Reply
12 Replies

5,942 Views
shrithi
Contributor I

Hi Chavira,

Can you provide I2c master flow diagram because slave is developed by us. So i can verify i2c master and slave flow is same.

The below i2c master driver used

drivers/i2c/busses/i2c-imx-lpi2c.c

0 Kudos
Reply

5,983 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @shrithi!

 

The device was added to the device tree?

Are you using i2c-tools to communicate with the device?

 

can you send a log file using the command i2cdetect?

 

Best Regards!

Chavira

0 Kudos
Reply

5,962 Views
shrithi
Contributor I

Hi Chavira

Yes, I have added slave device configuration in device-tree.

The slave address is ox3d.

i2cdetect -r -y 3
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- UU -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --

I have tried with i2cset and i2cget commands but i got below error
i2cset -y 3 0x3d 0x0 0x1
Error: Could not set address to 0x3d: Device or resource busy


Thanks,
Shrithi

0 Kudos
Reply

5,951 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @shrithi!


When a device shows UU instead of their direction under i2cdetect command, that means that device is being used by the kernel and that is the reason that you are getting the error.


I you want to use i2c tools to communicathe with the device you have to unload the module of the kernel that is using the device.


Try with the command insmod <name of module> and then you can use i2ctools.

Best regards!

Chavira

0 Kudos
Reply

5,945 Views
shrithi
Contributor I

Hi Chavira,

The i2c slave is mipi camera.
I have tried to i2c write through application which will call mipi ioctl and perform i2c write operation from driver.
You can refer the below
./mipi_config video_resolution_pattern selection 2 2 1
[ 55.546036] mipi_s_custom_ctrl
[ 55.549211] cid = 3 val = 34 reg = 0xb3b3
Resolution and video data pattern successfully

./mipi_config video_resolution_pattern selection 2 1 1
[ 103.514784] mipi_s_custom_ctrl
[ 103.517860] cid = 3 val = 33 reg = 0xb3b3
[ 104.526383] mipi_cam 3-003d: mipi_write_reg: error -110: reg=b3b3, val=21
Error setting pattern and resolution: Connection timed out 

Thanks,
Shrithi

0 Kudos
Reply

5,938 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @shrithi!

 

Dou you have the driver loaded by the kernel under device tree and at the same time do you want to write in i2c bus on the c application in user space?

 

 

0 Kudos
Reply

5,936 Views
shrithi
Contributor I
Hi Chavira,
 
Yes, the mipi camera is configured through I2C. Configuring through i2c is necessary whenever camera-related configurations are needed. The Ov5640 camera is an example.
 
The below is device-tree configuration
/* FPGA MIPI configuration */
&mipi_csi_0 { /* MIPI_CSI0: FPGA L MIPI TX */
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
 
port@0 {
reg = <0>;
mipi_csi0_ep: endpoint {
remote-endpoint = <&fpga_L_mipi_ep>;
data-lanes = <1 2 3 4>;
bus-type = <4>;
};
};
};
 
&i2c_mipi_csi0 { /* MIPI_CSI0: FPGA L TX */
#address-cells = <1>;
#size-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c_mipi_csi0>;
clock-frequency = <400000>;
status = "okay";
 
fpga_L_mipi: fpga_L_mipi@3d {
compatible = "iw,iw_mipi";
reg = <0x3D>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_mipi_csi0>;
mipi_csi;
status = "okay";
port {
fpga_L_mipi_ep: endpoint {
remote-endpoint = <&mipi_csi0_ep>;
data-lanes = <1 2 3 4>;
clocks-lanes = <0>;
};
};
};
};
 
Thanks,
Shrithi

 

 

0 Kudos
Reply

5,892 Views
Chavira
NXP TechSupport
NXP TechSupport

HI @shrithi!

 

For this case  I recommend to adjust your custom drivers.

 

To acces to the i2c bus you have 2 options, disable the kernel module to use the i2c tools or access to the bus using ioctl in a c program or adapt your driver to send and read the bus all in kernel, you can't do both.

 

Best Regards!

Chavira

0 Kudos
Reply

5,841 Views
shrithi
Contributor I

Hi Chavira,

I used the kernel to read and write i2c. I am facing an issue where the first I2C write will pass and the second I2C write will fail.  Can you provide an I2C master flow diagram?

Thanks,
Shrithi

0 Kudos
Reply

5,804 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @shrithi!

You can find a detailed flow described in Reference Manual on the chapter "5.8.2.2 Master Mode".

Chavira_0-1724078124800.png

 

You can find a detailed description of the driver in our Linux Reference Manual on chapter "4.6 Inter-IC (I2C)".

 

https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

 

Best Regards!

Chavira

0 Kudos
Reply

5,784 Views
shrithi
Contributor I

Hi Chavira,

Can you give i2c write and read timing diagram?

Thanks,
Shrithi

0 Kudos
Reply

5,751 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @shrithi!

 

You can find the table in datasheet.

 

Chavira_0-1724162147079.png

 

Chavira_1-1724162172764.png

 

Chavira_2-1724162207306.png

 

Best Regards!

Chavira

0 Kudos
Reply