I2C sequential Write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C sequential Write

Jump to solution
1,554 Views
Ludità
Contributor I

Messrs NXP,

I would ask to you if any device among #PCF8575, #PCA9535 & #PCA9555 does support I2C sequential write for an optimized data transfer in a point-to-point channel.

Best Regards

Tags (3)
0 Kudos
Reply
1 Solution
1,542 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

Please review the information below regarding the different devices:

PCF8575 - The devices supports sequential I2C writing procedure.

“The number of data bytes that can be sent successively is not limited. After every two bytes the previous data is overwritten.”

PCA9535 - The devices supports sequential I2C writing procedure.

“There is no limitation on the number of data bytes sent in one write transmission.”

PCA9555 - The devices supports sequential I2C writing procedure.

“There is no limitation on the number of data bytes sent in one write transmission. In this way, each 8-bit register may be updated independently of the other register..”

 

I do recommend to review the writing procedure of each device.

I hope this information helps.

Regards,

David

View solution in original post

0 Kudos
Reply
1 Reply
1,543 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

Please review the information below regarding the different devices:

PCF8575 - The devices supports sequential I2C writing procedure.

“The number of data bytes that can be sent successively is not limited. After every two bytes the previous data is overwritten.”

PCA9535 - The devices supports sequential I2C writing procedure.

“There is no limitation on the number of data bytes sent in one write transmission.”

PCA9555 - The devices supports sequential I2C writing procedure.

“There is no limitation on the number of data bytes sent in one write transmission. In this way, each 8-bit register may be updated independently of the other register..”

 

I do recommend to review the writing procedure of each device.

I hope this information helps.

Regards,

David

0 Kudos
Reply