How to start with IMX27 running Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to start with IMX27 running Linux

3,021 Views
helio
Contributor I
We would like to start a custom board design including an IMX27 chip.

I would like to know if there is some support for Linux in this processor and how to start with it.

Is the Linux BSP valid for custom board designs or only for ADS development board?

Thank you very much.

0 Kudos
Reply
3 Replies

1,066 Views
fabio_estevam
NXP Employee
NXP Employee
I would recommend you to download the Linux BSP for MX27ADS. You can use it as reference and adapt it for your custom hardware. It is available at: http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=02VS0l320822D0033202A7
 
Regards,
 
Fabio Estevam
0 Kudos
Reply

1,066 Views
helio
Contributor I
Thank you for your response.
As I have been reading trough the forum and documents, evaluation boards come with a flash with Redboot. And then, this loader lets you put kernel image in RAM or even in flash.

But, since we are using a custom board, we will have an empty flash. Is there any way to program the flash in a custom board with Redboot?

I have been searching for a tool called "HAB_toolkit". Is this suitable for this purpose?

Thank you very much.

0 Kudos
Reply

1,066 Views
fabio_estevam
NXP Employee
NXP Employee
You can use a JTAG for helping you during your board bring-up process.
 
 
(Click on IMX_ATK_TOOLKIT )
 
 
Regards,
 
Fabio Estevam
0 Kudos
Reply