How to enter the config mode of TJA1128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enter the config mode of TJA1128

Jump to solution
2,289 Views
asd046012
Contributor III

Hello

    Now I use TJA1128  as the Lin controller, and I want to enter the config mode of TJA1128,I see the data sheet, only when the CRC fail, TJA1128 will enter into config mode.

   So how to make CRC errors?

   

 

0 Kudos
Reply
1 Solution
2,283 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

NXP delivers the TJA1128 in the Config mode as initial mode.

If the device is programmed and is in Normal mode (or other) you can enter Config only by restoring factory preset value. The sequence is shown in Fig. 23 of the attached AH1801.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
1 Reply
2,284 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

NXP delivers the TJA1128 in the Config mode as initial mode.

If the device is programmed and is in Normal mode (or other) you can enter Config only by restoring factory preset value. The sequence is shown in Fig. 23 of the attached AH1801.

Best regards,

Tomas

0 Kudos
Reply