How to add a customized driver to Ltib kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add a customized driver to Ltib kernel

Jump to solution
4,450 Views
admin
Specialist II
I have been using Ltib for quite a while, but never touched its kernel customization.

I handed in a project recently. from kernel configuration GUI, I can see a driver had been added into kernel's driver list.

Since I need to add all the source into ClearCase for source control, I would like to learn, how a non-original driver been added in to kernel. is there a procedure to follow?

Thanks.
0 Kudos
Reply
1 Solution
1,967 Views
gaubuali01
Contributor III

where I can find this document ?

View solution in original post

0 Kudos
Reply
2 Replies
1,967 Views
fabio_estevam
NXP Employee
NXP Employee
You can refer to hello_mod package in LTIB. It shows an example of how to build and load a customer kernel module.
 
Regards,
 
Fabio Estevam
0 Kudos
Reply
1,968 Views
gaubuali01
Contributor III

where I can find this document ?

0 Kudos
Reply