Help running a standalone application on U-Boot based 8548 Power PC Target

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help running a standalone application on U-Boot based 8548 Power PC Target

4,455 Views
EricMT
Contributor I

My latest endaevor has me cross compiling a stand alone application for MPC8548 PPC for a U-Boot Based target.  There is no Operating System to run on the target to speak of, just my application.  I'm building the application in Code Warrior using an 8548_init.S hardware intialization file.

1) My first thought was that this should be as simple as using the .ELF image that codewarrior produces, right?  So I build a simple hello_world application and sent it down to my target.  U-Boot recognizes it as an ELF image, sets up the segements, and tries to run it!  But then low and behold, the U-Boot flash image comes up again. 

=> bootelf 400000
Loading .init @ 0x00002000 (972 bytes)
Loading .text @ 0x000023d0 (7624 bytes)
Loading .rodata @ 0x00004198 (256 bytes)
Loading .ctors @ 0x00004298 (8 bytes)
Loading .dtors @ 0x000042a0 (8 bytes)
Loading extab @ 0x000042a8 (16 bytes)
Loading extabindex @ 0x000042b8 (72 bytes)
Loading .data @ 0x00004300 (1024 bytes)
Loading .sdata @ 0x00004700 (44 bytes)
Clearing .sbss @ 0x00004730 (28 bytes)
Clearing .bss @ 0x00004750 (784 bytes)
Loading .abs.00000c00 @ 0x00000c00 (244 bytes)
## Starting application at 0x00002044 ...

U-Boot 1.3.0 (Jul 21 2008 - 12:20:51)

CPU:   8548_E, Version: 2.1, (0x80390021)
Core:  E500, Version: 2.2, (0x80210022)
Clock Configuration:

2) My next thought was to try and wrap it as a stand alone application image using "mkimage"  Ok, Great :smileyhappy:  To no avail....

$ mkimage -A ppc -O u-boot -T standalone -C none -a 2000 -e 2044 -n "Hiya stranger" -d debug.bin uDebug.bin              

## Total Size      = 0x00003ea0 = 16032 Bytes
=> bootm 400000
## Booting image at 00400000 ...
   Image Name:   Hiya stranger
   Image Type:   PowerPC U-Boot Standalone Program (uncompressed)
   Data Size:    15968 Bytes = 15.6 kB
   Load Address: 00002000
   Entry Point:  00002044
   Verifying Checksum ... OK
OK
**bleep**: 00000000 XER: 20000000 LR: 0FFD6378 REGS: 0ff9dc98 TRAP: 0700 DAR: 00000000
MSR: 00021200 EE: 0 PR: 0 FP: 0 ME: 1 IR/DR: 00

GPR00: 0FFD634C 0FF9DD88 00000200 00000001 0FFA048C 00000000 00005E5C 00000000
GPR08: 00000000 0FF9E00C 00000170 0FFD398C 0FF9DB70 0000C700 0FFF9A00 10040000
GPR16: 00000000 0FFEC9B4 00000000 00400040 00000001 00400000 00000000 00000001
GPR24: 0FFF52F8 0FFA0488 00000002 00002044 00400040 0FF9DF80 0FFFA2AC 00400000
** Illegal Instruction **
Call backtrace:
0FFD634C 0FFE3790 0FFE28E4 0FFE2D54 0FFD4600 0FFCABC8 0FFC162C
Program Check Exception
**bleep**: 0

How do I go about exporting my code warrior application so that I can run it as stand-alone on a U-Boot based target?  Thanks so much

0 Kudos
Reply
1 Reply

1,240 Views
medina
Contributor III
I supose Codewarrior doesn´t know that the u-boot is running. I think that U-BOOT has changed the immr´s address and your elf doesn´t find it, for exmaple.

You can debug your elf with codewarrior and usb-tap. By this way you can see the added code by codewarrior.


That is only a thought/suggestions. I hope help you.

Medina
0 Kudos
Reply