GD3160-Isolation failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GD3160-Isolation failure

1,340 次查看
irbaz7
Contributor I

I am using GD310 IC in one of the projects. The voltage on the LV side is 12V and the HV side is nearly 16 V.

What will be the impact if the isolation fails and is there any mechanism that can be implemented in traction inverter level to detect this ?

标记 (1)
0 项奖励
回复
1 回复

1,326 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Irbaz,

In any typical system which is fully isolated between HV and LV domains, a single point failure of the GD isolation will not create a functional issue (apart from high noise coupling). But this isolation failure would be a breach of the safety concept for human electrocution prevention. 

xavier_b_0-1736414374909.png

In practice, at GD level, most isolation failures will also result in other GD failures which will be detectable. However, as recommended in the safety manual, another means of ensuring the galvanic isolation integrity must be provided at system level. This is typically handled on the battery side, with dedicated leakage measurement circuitry, to ensure the maximum allowable leakage is not exceeded. (both polarities).

BRs, Tomas

0 项奖励
回复