GD3160-Isolation failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GD3160-Isolation failure

1,345件の閲覧回数
irbaz7
Contributor I

I am using GD310 IC in one of the projects. The voltage on the LV side is 12V and the HV side is nearly 16 V.

What will be the impact if the isolation fails and is there any mechanism that can be implemented in traction inverter level to detect this ?

タグ(1)
0 件の賞賛
返信
1 返信

1,331件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Irbaz,

In any typical system which is fully isolated between HV and LV domains, a single point failure of the GD isolation will not create a functional issue (apart from high noise coupling). But this isolation failure would be a breach of the safety concept for human electrocution prevention. 

xavier_b_0-1736414374909.png

In practice, at GD level, most isolation failures will also result in other GD failures which will be detectable. However, as recommended in the safety manual, another means of ensuring the galvanic isolation integrity must be provided at system level. This is typically handled on the battery side, with dedicated leakage measurement circuitry, to ensure the maximum allowable leakage is not exceeded. (both polarities).

BRs, Tomas

0 件の賞賛
返信