Freemaster forgetting max limit values for modifing variables.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Freemaster forgetting max limit values for modifing variables.

904 次查看
martinmeier
Contributor II

Everytime I restart Freemaster, even if saving the project (pmpx format in the latest version 1.4.4.4, Build Jan 13 2015 11:14:29), the max value for some of my modifiable variables are set the same as the minimum:

Clipboard03.png

That happens for both fractional and fixed point variables.

I've tried cloning and recreating the variables, with no success.

Is there a workaround for it?

Anyone else has this problem?

0 项奖励
回复
1 回复

804 次查看
martinmeier
Contributor II

New information I found: it only happens when the xml ".pmpx" format is used. When I use the ".pmp" it doesn't happen. So it's half a solution.