Freemaster forgetting max limit values for modifing variables.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster forgetting max limit values for modifing variables.

1,525 Views
martinmeier
Contributor II

Everytime I restart Freemaster, even if saving the project (pmpx format in the latest version 1.4.4.4, Build Jan 13 2015 11:14:29), the max value for some of my modifiable variables are set the same as the minimum:

Clipboard03.png

That happens for both fractional and fixed point variables.

I've tried cloning and recreating the variables, with no success.

Is there a workaround for it?

Anyone else has this problem?

0 Kudos
Reply
1 Reply

1,425 Views
martinmeier
Contributor II

New information I found: it only happens when the xml ".pmpx" format is used. When I use the ".pmp" it doesn't happen. So it's half a solution.