Flash programming operation failed When Flashing through Codewarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash programming operation failed When Flashing through Codewarrior

1,062 次查看
subashrajaram
Contributor I

Hi Folks,

Whenever I am trying to Flash the RCW and u-boot to the New board I am facing the following error.

(nor) fl_erase 0x0 0x1FFFF
Erasing...
Erased 128.00KB in 0.56s

(nor) fl_dump 0x0 0xFF
Dumping...
00000000: ffffffff ffffffff ffffffff ffffffff | ................
00000010: ffffffff ffffffff ffffffff ffffffff | ................
00000020: ffffffff ffffffff ffffffff ffffffff | ................
00000030: ffffffff ffffffff ffffffff ffffffff | ................
00000040: ffffffff ffffffff ffffffff ffffffff | ................
00000050: ffffffff ffffffff ffffffff ffffffff | ................
00000060: ffffffff ffffffff ffffffff ffffffff | ................
00000070: ffffffff ffffffff ffffffff ffffffff | ................
00000080: ffffffff ffffffff ffffffff ffffffff | ................
00000090: ffffffff ffffffff ffffffff ffffffff | ................
000000a0: ffffffff ffffffff ffffffff ffffffff | ................
000000b0: ffffffff ffffffff ffffffff ffffffff | ................
000000c0: ffffffff ffffffff ffffffff ffffffff | ................
000000d0: ffffffff ffffffff ffffffff ffffffff | ................
000000e0: ffffffff ffffffff ffffffff ffffffff | ................
000000f0: ffffffff ffffffff ffffffff ffffff | ...............
Dumped 255B in 0.30s

(nor) fl_write 0x0 /home/vchn144/Desktop/images/pbl_2bars_novf.bin --erase
Erasing from offset 0x0 864B
Writing...
Flash programming operation failed.
//
Additional error details:
[FP: program fail]

I have not faced this error before. I have googled regarding this and didn't get proper solution for this.

I am using Codewarrior 11.2.3  for linux . We are using LS2088A processor.

What may be the reason for the above one?

Thanks in Advance.

0 项奖励
回复
0 回复数