Flash programming operation failed When Flashing through Codewarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash programming operation failed When Flashing through Codewarrior

1,335件の閲覧回数
subashrajaram
Contributor I

Hi Folks,

Whenever I am trying to Flash the RCW and u-boot to the New board I am facing the following error.

(nor) fl_erase 0x0 0x1FFFF
Erasing...
Erased 128.00KB in 0.56s

(nor) fl_dump 0x0 0xFF
Dumping...
00000000: ffffffff ffffffff ffffffff ffffffff | ................
00000010: ffffffff ffffffff ffffffff ffffffff | ................
00000020: ffffffff ffffffff ffffffff ffffffff | ................
00000030: ffffffff ffffffff ffffffff ffffffff | ................
00000040: ffffffff ffffffff ffffffff ffffffff | ................
00000050: ffffffff ffffffff ffffffff ffffffff | ................
00000060: ffffffff ffffffff ffffffff ffffffff | ................
00000070: ffffffff ffffffff ffffffff ffffffff | ................
00000080: ffffffff ffffffff ffffffff ffffffff | ................
00000090: ffffffff ffffffff ffffffff ffffffff | ................
000000a0: ffffffff ffffffff ffffffff ffffffff | ................
000000b0: ffffffff ffffffff ffffffff ffffffff | ................
000000c0: ffffffff ffffffff ffffffff ffffffff | ................
000000d0: ffffffff ffffffff ffffffff ffffffff | ................
000000e0: ffffffff ffffffff ffffffff ffffffff | ................
000000f0: ffffffff ffffffff ffffffff ffffff | ...............
Dumped 255B in 0.30s

(nor) fl_write 0x0 /home/vchn144/Desktop/images/pbl_2bars_novf.bin --erase
Erasing from offset 0x0 864B
Writing...
Flash programming operation failed.
//
Additional error details:
[FP: program fail]

I have not faced this error before. I have googled regarding this and didn't get proper solution for this.

I am using Codewarrior 11.2.3  for linux . We are using LS2088A processor.

What may be the reason for the above one?

Thanks in Advance.

0 件の賞賛
返信
0 返答(返信)