Flash Programmer Device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Programmer Device

3,522 Views
rogelio_rafael
Contributor I

Hi.

I need your support, we are currently developing a programming station for a production line.

Please, you can help me select a programmer device with support to flash the MWCT1013VLH IC.

The programmer device may be to use in Windows 7 or latter.

If is required more information we are you service to shared.

0 Kudos
Reply
7 Replies

3,400 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Rogelio,

Regarding your question, of course, the CodeWarrior for mcu ver11.x tools provides the Flash programming function, pls refer to the following screenshot:

Pls have a try.

BR

XiangJun Rong

pastedImage_1.png

0 Kudos
Reply

3,400 Views
rogelio_rafael
Contributor I

Hi xiangjun.rong thank you for the answer,

One question, what is the model or part numbert of programmer device used to flash the MWCT1013VLH IC.?

Best Regards

Rogelio R

0 Kudos
Reply

3,400 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

After you click the "Flash File to Target", you can follow up  the the following configuration to erase/program the application for the MWCT1013VLH IC.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 Kudos
Reply

3,400 Views
rogelio_rafael
Contributor I

Hi xiangjun.rong thank you for the answer,

 

What is the model of programmer device used or with coverage to flash the MWCT1013VLH IC.??

Some example of other programmer device models: (But this devices not have a coverage for flash the MWCT1013VLH IC).

Flash Runner FR Cube

Algocraft

Renessas FP-5

 

Best Regards

Rogelio R

0 Kudos
Reply

3,400 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Rogelio,

As you know all the following tools are third party tools, I am not sure if they can program flash of MWCT1013VLH IC, I think the MWCT1013VLH IC. is the same as MC56F84789, if it includes the MC56F84789, it is okay.

Flash Runner FR Cube

Algocraft

Renessas FP-5

BR

XiangJun Rong

0 Kudos
Reply

3,400 Views
rogelio_rafael
Contributor I

Hi xiangjun.rong thank you for the answer again,

I am would like adquire a programmer tool for flashing the MWCT1013VLH IC, of NXP but i not shure which tool adquire.

Can you recommend some model of tool, please.?

Best Regards
Rogelio Rafael

0 Kudos
Reply

3,400 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Rogelio,

The CodeWarrior for MCU ver11.x tools provides the tools to program on-chip flash of MWCT1013VLH, have you tried to use it?

Regarding the third party tools, I am not familiar with.

BR

Xiangjun Rong

0 Kudos
Reply