First byte of Random UID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

First byte of Random UID

ソリューションへジャンプ
2,496件の閲覧回数
dharmikm91
Contributor I

Hello, I am trying to authenticate a DESfire card using the Pegoda. For my application, I need it to use the Random UID and not the card UID. According to the documentation in MF3ICD81 (Product Data Sheet) and AN10927, if we set the card to use Random UID using 'SetConfiguration' command, it will assign the first byte as 0x08. However, when I am trying to get the Random UID on my Pegoda, the first byte of the 4-Byte Random UID is 0x80 which is causing my tests to fail.

Can you please help me out? 

Thanks in advance.

0 件の賞賛
返信
1 解決策
2,477件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Mifare Desfire EV1 with random id enabled UID0 should is 0x80. Please find the more information as the thread.https://community.nxp.com/t5/NFC/Identification-of-Random-ID/m-p/809492.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,478件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Mifare Desfire EV1 with random id enabled UID0 should is 0x80. Please find the more information as the thread.https://community.nxp.com/t5/NFC/Identification-of-Random-ID/m-p/809492.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信