FXLS8974CF Accelerometer Package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FXLS8974CF Accelerometer Package

ソリューションへジャンプ
2,746件の閲覧回数
David-G
Contributor I

We have added the FXLS8974CF to a new PCB design using the VSON10 package (SOT1615-3). However the distributer is offering us the FXLS8974CFR3, which uses the DFN-10 package, according to section 4.1 Ordering Options (table 2, page 2) in the datasheet.

Question: What does the suffix 'R3' stand for and is the DFN-10 package the same as VSON10 (SOT1615-3) ?

0 件の賞賛
返信
1 解決策
2,727件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello David,

The terminology is confusing. Sorry for that.

DFN-10 is just a generic abbreviation for a 10pin DFN package. VSON10 (SOT1615-3) is (I believe) a more specific identifier.

What I can say is that FXLS8962AF, FXLS8964AF, FXLS8967AF, FXLS8974CF all have the same identical package.

The R3 is a reel designator. We are starting to standardize on R1 -> 1k reel and R3 -> 3k reel. FXLS8964AFR3, FXLS8967AFR3, FXLS8974CFR3 all are launching with only one reel size option (3k reel).

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,728件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello David,

The terminology is confusing. Sorry for that.

DFN-10 is just a generic abbreviation for a 10pin DFN package. VSON10 (SOT1615-3) is (I believe) a more specific identifier.

What I can say is that FXLS8962AF, FXLS8964AF, FXLS8967AF, FXLS8974CF all have the same identical package.

The R3 is a reel designator. We are starting to standardize on R1 -> 1k reel and R3 -> 3k reel. FXLS8964AFR3, FXLS8967AFR3, FXLS8974CFR3 all are launching with only one reel size option (3k reel).

Best regards,

Tomas

0 件の賞賛
返信
2,724件の閲覧回数
David-G
Contributor I

Hi Tomas

Thank you for your explanation, much appreciated.

Best Regards, David

0 件の賞賛
返信