FS6510 Level Triggering at low level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS6510 Level Triggering at low level

Jump to solution
2,321 Views
N123
Contributor II

Hi,

Is it possible configure a low-level trigger on IO of FS6510 SBC for waking up?

We want to use level triggering but below a voltage.

For example, whenever IO5 receives a level lower than 5V, then it should wake up the system. (We don’t want to depend on edge triggering as we are unsure on rate of falling).

In case there is some documentation stating all register definitions, please share.

0 Kudos
Reply
1 Solution
2,297 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Neetigya,

I do not have such data. I can only add an info about the deglitch time:

Deglitch.JPGDeglitch.JPG

Meaning, if IO voltage < 2.1V and the duration is > 70us, then the device will wake up. 

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
4 Replies
2,310 Views
N123
Contributor II

Hi,

Thank you. Could you please share edge triggered data similar way? Like voltage levels and rate of rise and fall (as in 2nd screenshot)? 

 

0 Kudos
Reply
2,298 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Neetigya,

I do not have such data. I can only add an info about the deglitch time:

Deglitch.JPGDeglitch.JPG

Meaning, if IO voltage < 2.1V and the duration is > 70us, then the device will wake up. 

Best regards,

Tomas

0 Kudos
Reply
2,294 Views
N123
Contributor II

Hi, Thank you very much.

We were asking regarding this time constraint only.

0 Kudos
Reply
2,313 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Neetigya,

Yes, it is possible to achieve that by setting WU_IO5_1:0 bits to 0b10:

WU.JPGWU.JPG

Valid high/low voltage: IO5 pin Voltage>2.6V = High, Voltage<2.1V = Low:

Digital Input.JPGDigital Input.JPG

Best regards,

Tomas

0 Kudos
Reply